Re: Which ECC i.MX6 ROM code uses?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Which ECC i.MX6 ROM code uses?

ソリューションへジャンプ
2,238件の閲覧回数
abdulrasheed
Contributor I

YuriMuhin_ng‌ I used your attached BCH_enco.c and found that it generates incorrect code for some data blocks.
is there any updated version of this file is available?
This file generated incorrect/different ECC for program_image as compare to ECC generated by kobs-ng utility for NAND.

0 件の賞賛
返信
1 解決策
2,122件の閲覧回数
b36401
NXP Employee
NXP Employee

The algorithm Yuri attached is one used on i.MX6 processors.
And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.
Please make sure that you set right parameters for encoding algorithm.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,122件の閲覧回数
b36401
NXP Employee
NXP Employee

Additionally to doublecheck if it is right algorithm please create a technical case:
https://community.nxp.com/thread/381898
I will attach the file.

0 件の賞賛
返信
2,123件の閲覧回数
b36401
NXP Employee
NXP Employee

The algorithm Yuri attached is one used on i.MX6 processors.
And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.
Please make sure that you set right parameters for encoding algorithm.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信