Re: Question about OCRAM_PXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Question about OCRAM_PXP

1,094 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Thank you for reply.

Could you tell me more detail about "a mode where the internal RAM serves as frame buffer to minimize external memory bandwidth.” ?

I can't image the mode of it.

Furthermore, do you have any sample or document to use other internal RAM such as OCRAM ?

My customer want to reduce the access load to the external RAM.

Ko-hey

0 Kudos
Reply
1 Reply

1,027 Views
Yuri
NXP Employee
NXP Employee

Hello,

   please refer to section 13.7.3.30 (LCDIF Handshake) of i.MX7D RM.

https://www.nxp.com/docs/en/reference-manual/IMX7DRM.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply