Re: PCIe EP DMA write to i.MX6 RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: PCIe EP DMA write to i.MX6 RAM

1,273 Views
egabay1
Contributor I

Thanks Jaime,

To be more specific regarding my question, does the EP write access to the i.MX6 DDR memory managed by a DMA controller (for CPU core offload)?

 According to Table 3-2.  SDMA event mapping, in the i.MX6 i.MX 6Dual/6Quad Applications Processor Reference Manual, the PCIe is not mentioned as one of the i.MX6 DMA controller (SDMA) request signals.

Eyal

0 Kudos
Reply
1 Reply

1,180 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The configuration, shown in https://community.nxp.com/docs/DOC-95014 

uses IPU DMA abilities.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply