Re: LTIB for i.mx28?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: LTIB for i.mx28?

1,041 次查看
tomhanks
Contributor I

Hey, thanks for the update.  that worked.  but now I have another issue.  When I do ./ltib, I get this error in the host_config.log file.  Any idea?  Is this the right forum to post to for this?

gcc conf.o zconf.tab.o -o conf
zconf.tab.o: In function `menu_re_search':
/opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:416: undefined reference to `next_id'
/opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:427: undefined reference to `next_id'
collect2: error: ld returned 1 exit status
Makefile:106: recipe for target 'conf' failed
make: *** [conf] Error 1
error: Bad exit status from /home/twhanks/Wolf/ltib/tmp/rpm-tmp.92159 (%build)


RPM build errors:
Bad exit status from /home/twhanks/Wolf/ltib/tmp/rpm-tmp.92159 (%build)
Build time for lkc: 1 seconds

Failed building lkc
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554


Started: Wed May 10 14:19:37 2017
Ended: Wed May 10 14:21:29 2017
Elapsed: 112 seconds

These packages failed to build:
lkc

0 项奖励
回复
1 回复

830 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  the following app note may be helpful :

"Building for i.MX Mature Boards"

http://www.nxp.com/docs/en/application-note/AN12024.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复