Re: HAB issue i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: HAB issue i.MX6UL

Jump to solution
1,630 Views
PramodKumar
Contributor IV

Hiii Yuri ,

This is the output I am getting I think this one is an issue , if , then how to resolve it .

> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x24 0x42 0x33 0x30 0xc0 0x1d
0x00 0x08 0x00 0x02 0x40 0x00 0x05 0x16
0x55 0x55 0x00 0x0f 0x17 0x7f 0xf4 0x00
0x00 0x00 0x00 0x02 0xc0 0x00 0x08 0x40
0x00 0x00 0x00 0x05

--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00
0x00 0x00 0x00 0x20

--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x2c
0x00 0x00 0x01 0xe0

--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20
0x00 0x00 0x00 0x01

--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00
0x00 0x00 0x00 0x04

Regards ,

Pramod

0 Kudos
Reply
1 Solution
1,504 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 “Appendix A: Interpreting HAB Event Data from Report_Event() API”

of “HAB4_API.pdf” in the CST 3.1.0 package shows how to interpret

hab events.

  I will send more details via e-mail.


Have a great day,
Yuri.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,505 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 “Appendix A: Interpreting HAB Event Data from Report_Event() API”

of “HAB4_API.pdf” in the CST 3.1.0 package shows how to interpret

hab events.

  I will send more details via e-mail.


Have a great day,
Yuri.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply