Re: 3 Wire SPI Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: 3 Wire SPI Working

14,085件の閲覧回数
mohammedazlum
Contributor IV

Hello Mohammed,

Could you tell me that, how did you connect 3-wire SPI into iMX6x processor ? The output/input line from the slave connected to which pin of processor (whether MISO or MOSI) ?

3 wire SPI.png

Regards,

Azlum

0 件の賞賛
返信
18 返答(返信)

11,896件の閲覧回数
jamesdeepu
Contributor II

Dear Azlum,

I am also working on 3-Wire SPI. I read your posts. Can you clarify my doubts.

I have imx6 board with MOSI and MISO both Connected to SDI and SDO of LCD (Slave device).

On the slave side , SDO and SDI are connected together  where SDO is connected via a resistor

My query is

1) How will I tell linux kernel to use SPI-3 Wire mode

2) As per your previous discussion, MOSI should be connected via a resistor.?

3) In my case MISO is connected to SDO which is connected to SDI via a resistor(different from your case). Will that work out?

4) Bitbanging is only required if I don t connect MOSI to MISO via a resistor ?

pastedImage_0.png

Thanks in advance

0 件の賞賛
返信

11,896件の閲覧回数
ask
Contributor III

Hi Mohammad,

We have imx28 customized board. LCDIF was interfaced to 3 wire spi display panel. The input/output line from the slave connected to both the pins i.e MISO and MOSI. Even in your case it should be connected like that.

0 件の賞賛
返信

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Ask,

Could you share the schematic portion to me ? Did you short MISO and MOSI of iMX6 and finally connected to 3-wire Slave bidirectional data line?

Regards,

Azlum

0 件の賞賛
返信

11,896件の閲覧回数
ask
Contributor III

Hi Mohammed,


We did n't use the iMx6 and used imx28.
In my case slave is a output device and has unidirectional communication. Slave data input/output connected to MISO and MOSI pins of a Master.

0 件の賞賛
返信

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Ask,

If slave is output device, why did you short MISO and MOSI together? I think you can connect salve output line to MISO directly and leave MOSI as open.

Regards,

Azlum

0 件の賞賛
返信

11,896件の閲覧回数
Yuri
NXP Employee
NXP Employee

  To avoid contention, output signals / pins should be configured as open drain.
It may be done for any pin functionality. 

Regards,

Yuri.

0 件の賞賛
返信

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Yuri,

If I configure MISO and MOSI as open drain, then the Master and Slave communication will be out of SPI protocol.

i.e, one side (Slave side) is 3-wire SPI interface and another side (Master side) is open drain interface.

Whether my statement is correct ?


Regards,

Azlum

0 件の賞賛
返信

11,896件の閲覧回数
Yuri
NXP Employee
NXP Employee

The open drain just provides physical level of a communication protocol.

Regards,

Yuri. 

0 件の賞賛
返信

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Yuri,

i.e iMX6 SPI MOSI and MISO short together and configure MOSI as open-drain mode. In other words, SPI with MOSI open-drain mode.

What about MISO ? No need to configure as anything ?

Based on your input I modified my wiring diagram. Can you review the same ?

SPI-3 wire open mode.png

Regards,

Azlum

0 件の賞賛
返信

11,896件の閲覧回数
Yuri
NXP Employee
NXP Employee

> What about MISO ? No need to configure as anything ?


Correct, no need to configure input.

Regards,

Yuri.

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Yuri,

When MOSI drive signal, the same signal can be feed into slave input and MISO of master. Is it create any problem or conflict ?

Regards,

Azlum

0 件の賞賛
返信

11,896件の閲覧回数
Yuri
NXP Employee
NXP Employee

I do not think so.

~Yuri.

0 件の賞賛
返信

11,896件の閲覧回数
mohammedazlum
Contributor IV

Hi Yuri, Thank you for the reply....


After configure MOSI as open-drain, do we need to use Bit-Banging Technique ?


Regards,

Azlum

0 件の賞賛
返信

11,897件の閲覧回数
Yuri
NXP Employee
NXP Employee

No bit-banging needed. But pull up resistors (as for I2C) should be provided.

~Yuri.

0 件の賞賛
返信

11,897件の閲覧回数
mohammedazlum
Contributor IV

Hello Yuri,

So iMX6x MISO and MOSI need to be shorted together and finally connect to 3-wire SPI slave bidirectional data line (I/P & O/P line). Is it like that ?

Then MOSI need to be configured as GPIO. Then what about MISO ? This pin no need to configure as anything ?

Regards,

Azlum

0 件の賞賛
返信

11,873件の閲覧回数
Halotem12
Contributor I

iMX6x MISO and MOSI need to be shorted I have the same 3 wire spi connection in my application

0 件の賞賛
返信

11,897件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Assuming i.MX6 is SPI master, You may configure its MOSI output as open drain one
(via ODE bit field of corresponding IOMUXC_SW_PAD_CTL_PAD register) and
connect together i.MX6 MOSI, MISO and external SPI device I/O [I/P & O/P].

If needed, external device I/O should be configured for open drain too.

  When configuring GPIO, the Processor Expert for i.MX  may be useful.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX

https://community.freescale.com/docs/DOC-101470

Also, the following app note helps to setup pin’s electrical properties.

“Influence of Pin Setting on System Function and Performance”

  http://www.freescale.com/files/32bit/doc/app_note/AN5078.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

11,897件の閲覧回数
soledad
NXP Employee
NXP Employee

jamesbone , Can you please help?

0 件の賞賛
返信