Random stop audio playback on SGTL5000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Random stop audio playback on SGTL5000

2,308 次查看
giacomomola
Contributor II

Hello,
I have a custom board with imx28 (287) and sgtl5000, kernel 4.
sound codec sgtl5000.

while in playback while performing a song at random
the audio stops feeling.

the kernel hooks the codec properly start and for a while everything seems to work as it should.

some advice??

thank you

excuse for my easy english

Giacomo

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

2,013 次查看
art
NXP Employee
NXP Employee

It might be the effect of the SGTL5000 silicon erratum in case of using the internal VDDD regulator. Please check. The erratum itslef is described in the SGTL5000 Silicon Errata document, available on the SGTL5000 Documentation web page:

http://www.nxp.com/products/media-and-audio-processing/data-converters/audio-converters/audio-codec/...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,013 次查看
giacomomola
Contributor II

Hello,
the problem was derived from a grounded inductor disorders and cleared it led into the chip.
solved

thank you
regards

Giacomo

0 项奖励
回复

2,013 次查看
giacomomola
Contributor II

I verified,
when he stops playing records

ANA_CTRL (0x0024) and ANA_POWER (0x0030) of SGTL return to their default values 0x0111 and 0x7060, with devices switched off.

why can go to reset or return to the default values in those registers

thank you

Giacomo

0 项奖励
回复