Random crashes at boot-up in 3.10.17 kernel when all 4 cores of iMX6Q based custom board are enabled.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Random crashes at boot-up in 3.10.17 kernel when all 4 cores of iMX6Q based custom board are enabled.

995 Views
zaheerm
Contributor I

We are facing random crashes at boot-up when we enable all the 4 cores on a iMX6Q based custom board.

The kernel boots with upto 3 cores correctly, without any crashes.

Let us know if any one has come across the issue and has a resolution.

Labels (2)
0 Kudos
Reply
1 Reply

850 Views
igorpadykov
NXP Employee
NXP Employee

He Zaheer

please try to narrow down by running software on Freescale reference

board. If this will work well, then it is probably power supplies issue

(ripples, noise, e.t.c.).

If you are sure that this is specific 3.10.17 issue please post this to

meta-fsl-arm mailing list, to our code developers.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply