Random crash at imx6dl with Android 4.4.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Random crash at imx6dl with Android 4.4.2

跳至解决方案
3,816 次查看
denniswang_tw
Contributor II

Dear all,

i'm developing on a custom imx6dl-based board.

The kernel version is 3.0.35.

We found a problem that android will reboot randomly when application/dialog pop up.

It always happened after power on and enter first app from launcher.

is this a known issue ? Or any suggestion to find the RC?

Thanks.

[09/18/15 Abnormal]-S-| Unable to handle kernel NULL pointer dereference at virtual address 00000010

                      | pgd = b8dcc000

                      | [00000010] *pgd=00000000

                      | Internal error: Oops: 805 [#1] PREEMPT SMP

                      | Modules linked in: wl12xx_sdio wl12xx mac80211 cfg80211 compat

                      | CPU: 0    Not tainted  (3.0.35-r4.4.2 #10)

                      | PC is at _Split+0xa4/0xbc

                      | LR is at __kmalloc+0x44/0x140

                      | pc : [<8041c8d0>]    lr : [<800ecb50>]    psr: 60010013

                      | sp : b87a9cc0  ip : 01100000  fp : b87a9ce4

                      | r10: 00000000  r9 : 00000002  r8 : b87a9cfc

                      | r7 : bc162e00  r6 : 00012000  r5 : 00000001  r4 : bc162e00

                      | r3 : bc072a80  r2 : 00000000  r1 : 80791ca0  r0 : 00000000

                      | Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

                      | Control: 10c53c7d  Table: 48dcc04a  DAC: 00000015

                      |

                      | PC: 0x8041c850:

                      | c850  0a000021 e5913018 e1560003 8a00001e e3a01074 e24b2020 ebffccf3 e1500005

                      | c870  ba000019 e51b3020 e5942014 e0862002 e5832014 e5942018 e583501c e5835020

                      | c890  e0662002 e5832018 e3a05001 e5942000 e5832000 e5942024 e5832024 e5942028

                      | c8b0  e5832028 e5942004 e9830014 e5823008 e594200c e5843004 e5834010 e583200c

                      | c8d0  e5823010 e584300c e5846018 e1a00005 e24bd018 e89da870 e1a0c00d e92ddff0

                      | c8f0  e24cb004 e24dd014 e2528000 e3a05000 e1a07000 e1a0c001 e1a0a003 e50b5030

                      | c910  0a000030 e1530005 0a00002e e5906004 e3a01074 e24b2030 e50bc038 e1a00006

                      | c930  ebffccc1 e51bc038 e2509000 ba000026 e51b4030 e2840048 e8841080 e5845010

                      |

                      | LR: 0x800ecad0:

                      | cad0  e3a02002 ebffff8e e89da800 e1a0c00d e92dd800 e24cb004 e3a0200a ebffff88

                      | caf0  e89da800 e1a0c00d e92dd800 e24cb004 e3a02009 ebffff82 e89da800 e1a0c00d

                      | cb10  e92dddf0 e24cb004 e3500a02 e1a06001 9a000009 e2403001 e3e01000 e1a035a3

                      | cb30  e1b030a3 e2811001 1afffffc e3860901 ebff68ca e1a04000 ea00003c ebfffd0f

                      | cb50  e3500010 e1a04000 9a000038 e1a0200d e59f10e0 e3c23d7f e3c3303f e5930014

                      | cb70  e5942000 e7910100 e082c000 e59c8004 e7925000 e3550000 1a000004 e1a00004

                      | cb90  e1a01006 eb137162 e1a05000 ea00001b e10f0000 f10c0080 e593c014 e5947000

                      | cbb0  e791c10c e1a02007 e792a00c e15a0005 1a00000e e2877004 e797700c e1570008

                      |

                      | SP: 0xb87a9c40:

                      | 9c40  00000001 8005074c b87a8000 00000000 b87a9c74 b87a9c60 ffffffff b87a9cac

                      | 9c60  00012000 bc162e00 b87a9ce4 b87a9c78 8005066c 8004b3dc 00000000 80791ca0

                      | 9c80  00000000 bc072a80 bc162e00 00000001 00012000 bc162e00 b87a9cfc 00000002

                      | 9ca0  00000000 b87a9ce4 01100000 b87a9cc0 800ecb50 8041c8d0 60010013 ffffffff

                      | 9cc0  00012000 bc072a80 bc6d4f00 bca8bc00 00012000 00000040 b87a9d2c b87a9ce8

                      | 9ce0  8041ced0 8041c838 b87a9cfc b87a9cf8 80095a88 bc6d4f00 b87a9d14 00000000

                      | 9d00  8040f638 00000000 b87a9de0 00000006 bc6d4f00 00012000 0000000a 00000002

                      | 9d20  b87a9dbc b87a9d30 80415460 8041cd58 00000002 b87a9d6c 00000000 00000000

                      |

                      | FP: 0xb87a9c64:

                      | 9c64  bc162e00 b87a9ce4 b87a9c78 8005066c 8004b3dc 00000000 80791ca0 00000000

                      | 9c84  bc072a80 bc162e00 00000001 00012000 bc162e00 b87a9cfc 00000002 00000000

                      | 9ca4  b87a9ce4 01100000 b87a9cc0 800ecb50 8041c8d0 60010013 ffffffff 00012000

                      | 9cc4  bc072a80 bc6d4f00 bca8bc00 00012000 00000040 b87a9d2c b87a9ce8 8041ced0

                      | 9ce4  8041c838 b87a9cfc b87a9cf8 80095a88 bc6d4f00 b87a9d14 00000000 8040f638

                      | 9d04  00000000 b87a9de0 00000006 bc6d4f00 00012000 0000000a 00000002 b87a9dbc

                      | 9d24  b87a9d30 80415460 8041cd58 00000002 b87a9d6c 00000000 00000000 00000002

                      | 9d44  00000040 00000000 00000000 00000000 00000000 00000000 0000084c 2d1d455f

                      |

                      | R1: 0x80791c20:

                      | 1c20  80791c20 80791c20 80791c28 80791c28 00000000 00000000 80791c38 80791c38

                      | 1c40  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

                      | 1c60  00000064 81158040 00008000 0000000f 81158060 00000008 00000002 81158020

                      | 1c80  81149000 0000002c 81150000 81158000 00000001 00001000 00000000 00000001

                      | 1ca0  01100000 01108000 00000000 00000000 00000000 00000002 0004effb 0004ffff

                      | 1cc0  00000001 00000032 0000fffa 00000001 bc02be80 bc002200 bc003700 00000003

                      | 1ce0  bc00d460 bc002200 bc003600 00000011 8115c160 0001ffff 00000064 bc002580

                      | 1d00  00000010 0000ffff 811dc160 bc003680 00100000 bc00c000 00000003 bc003700

                      |

                      | R3: 0xbc072a00:

                      | 2a00  f0000870 00000007 bc072a60 0002416d 00000000 00000000 00000000 00000000

                      | 2a20  805dc300 805dc280 bc037a80 bc037800 00000000 00000000 00000000 00000000

                      | 2a40  00000001 00000000 00000000 00000000 00000000 bc072a54 bc072a54 00000000

                      | 2a60  2d786d69 00633269 bc15cef8 8009e824 ffffffff ffffffff ffffffff ffffffff

                      | 2a80  bca8bc00 bde1d880 bc162e00 00000000 bc162e00 00432000 0034a000 00000000

                      | 2aa0  00000000 00000006 00000000 00000000 00000000 00000000 00000000 00000000

                      | 2ac0  00000000 fffffff0 00000000 00000000 00000000 b8c96980 00000000 bde18200

                      | 2ae0  807a5518 bc25b900 b932faa0 8009e824 65732074 63697672 00000065 00000000

                      |

                      | R4: 0xbc162d80:

                      | 2d80  00000002 00000000 00000000 00000000 00000000 00000000 00000000 00000000

                      | 2da0  00000000 00000000 00000000 00000000 ffffffff ffffffff ffffffff ffffffff

                      | 2dc0  ffffffff ffffffff 00000000 00000000 00000000 bc187580 00000000 807a5730

                      | 2de0  807a5518 807a5e48 00000000 00000000 ffffffff ffffffff ffffffff ffffffff

                      | 2e00  bca8bc00 bc072a80 bc634700 00000000 00000000 00420000 0035c000 00000000

                      | 2e20  00000001 00000006 00000000 00000000 00000000 ffffffff ffffffff ffffffff

                      | 2e40  ffffffff ffffffff 00000001 00000000 00000000 00000000 00000006 807a5730

                      | 2e60  807a5518 807a5e48 bc160b18 8009e824 054ae8bf 00000008 00000000 ffffffff

                      |

                      | R7: 0xbc162d80:

                      | 2d80  00000002 00000000 00000000 00000000 00000000 00000000 00000000 00000000

                      | 2da0  00000000 00000000 00000000 00000000 ffffffff ffffffff ffffffff ffffffff

                      | 2dc0  ffffffff ffffffff 00000000 00000000 00000000 bc187580 00000000 807a5730

                      | 2de0  807a5518 807a5e48 00000000 00000000 ffffffff ffffffff ffffffff ffffffff

                      | 2e00  bca8bc00 bc072a80 bc634700 00000000 00000000 00420000 0035c000 00000000

                      | 2e20  00000001 00000006 00000000 00000000 00000000 ffffffff ffffffff ffffffff

                      | 2e40  ffffffff ffffffff 00000001 00000000 00000000 00000000 00000006 807a5730

                      | 2e60  807a5518 807a5e48 bc160b18 8009e824 054ae8bf 00000008 00000000 ffffffff

                      |

                      | R8: 0xb87a9c7c:

                      | 9c7c  80791ca0 00000000 bc072a80 bc162e00 00000001 00012000 bc162e00 b87a9cfc

                      | 9c9c  00000002 00000000 b87a9ce4 01100000 b87a9cc0 800ecb50 8041c8d0 60010013

                      | 9cbc  ffffffff 00012000 bc072a80 bc6d4f00 bca8bc00 00012000 00000040 b87a9d2c

                      | 9cdc  b87a9ce8 8041ced0 8041c838 b87a9cfc b87a9cf8 80095a88 bc6d4f00 b87a9d14

                      | 9cfc  00000000 8040f638 00000000 b87a9de0 00000006 bc6d4f00 00012000 0000000a

                      | 9d1c  00000002 b87a9dbc b87a9d30 80415460 8041cd58 00000002 b87a9d6c 00000000

                      | 9d3c  00000000 00000002 00000040 00000000 00000000 00000000 00000000 00000000

                      | 9d5c  0000084c 2d1d455f 807cffc0 bca8bc00 00000000 007fffff 53431000 00000000

                      | Process til.saioutility (pid: 2124, stack limit = 0xb87a82f8)

                      | Stack: (0xb87a9cc0 to 0xb87aa000)

                      | 9cc0: 00012000 bc072a80 bc6d4f00 bca8bc00 00012000 00000040 b87a9d2c b87a9ce8

                      | 9ce0: 8041ced0 8041c838 b87a9cfc b87a9cf8 80095a88 bc6d4f00 b87a9d14 00000000

                      | 9d00: 8040f638 00000000 b87a9de0 00000006 bc6d4f00 00012000 0000000a 00000002

                      | 9d20: b87a9dbc b87a9d30 80415460 8041cd58 00000002 b87a9d6c 00000000 00000000

                      | 9d40: 00000002 00000040 00000000 00000000 00000000 00000000 00000000 0000084c

                      | 9d60: 2d1d455f 807cffc0 bca8bc00 00000000 007fffff 53431000 00000000 807d0a40

                      | 9d80: 00000002 00000000 b87a9e2c b87a9d98 800c6908 bc665000 b87a8000 00007530

                      | 9da0: b91b8020 00000000 b87a8000 00000000 b87a9efc b87a9dc0 8040f0ac 80414e24

                      | 9dc0: 7e8aa040 00000000 000000f8 00000000 7e8aa040 00000000 000000f8 00000000

                      | 9de0: 00000007 00000001 5342e008 7e8aa7c8 0000ac40 00000000 7e8aa648 00000000

                      | 9e00: 00012000 00000040 00000002 00000001 0000084c 00000000 00000000 7e8aa648

                      | 9e20: 00000001 00000000 5342e008 00001380 00000007 2c016008 00000008 0000000b

                      | 9e40: 00000008 00000008 00000047 000000b9 00000001 2b0d6924 2c016008 00000100

                      | 9e60: 00000100 2b0d6a10 00000034 0000b900 ffffffff 00000000 7e8aafe8 7e8aa858

                      | 9e80: 0000ab80 00000000 7e8aa6d8 00000000 000000c0 55fb5780 55fb5780 53014d3b

                      | 9ea0: 7e8aa918 0000000c 00000001 7e8aa6d8 00000001 00000000 7e8aafe8 2b0d6924

                      | 9ec0: 2c016008 0000000c 0000000a 2b0d6e0c 00000a54 00000038 bd83dd08 7e8a9fe0

                      | 9ee0: b8d35320 00000026 00000000 00000000 b87a9f74 b87a9f00 800ffc78 8040eefc

                      | 9f00: 8004b40c 80058924 8009d930 800bdf10 00000000 81152090 bd91c01c b8772a00

                      | 9f20: bcf529c0 b87a8000 b87a9f4c b87a9f38 8009d95c 8009d8f4 8004a040 b8772a00

                      | 9f40: 00000001 b8d35320 b87a9f74 b87a9f58 b8d35320 7e8a9fe0 00007530 00000026

                      | 9f60: 00000000 b87a8000 b87a9fa4 b87a9f78 800ffd44 800ff72c b87a9f94 00000001

                      | 9f80: 80095a88 00002710 00007530 53056ee8 00000036 80050d84 00000000 b87a9fa8

                      | 9fa0: 80050c00 800ffcf8 00002710 00007530 00000026 00007530 7e8a9fe0 7e8a9fc8

                      | 9fc0: 00002710 00007530 53056ee8 00000036 7e8aa178 00012000 00000068 5348ab18

                      | 9fe0: 5348caa8 7e8a9fb8 2abfc23b 2abef664 40010010 00000026 00000000 00000000

                      | Backtrace:

                      | [<8041c82c>] (_Split+0x0/0xbc) from [<8041ced0>] (gckVIDMEM_AllocateLinear+0x184/0x220)

                      |  r6:00000040 r5:00012000 r4:bca8bc00

                      | [<8041cd4c>] (gckVIDMEM_AllocateLinear+0x0/0x220) from [<80415460>] (gckKERNEL_Dispatch+0x648/0x1578)

                      | [<80414e18>] (gckKERNEL_Dispatch+0x0/0x1578) from [<8040f0ac>] (drv_ioctl+0x1bc/0x274)

                      | [<8040eef0>] (drv_ioctl+0x0/0x274) from [<800ffc78>] (do_vfs_ioctl+0x558/0x5cc)

                      | [<800ff720>] (do_vfs_ioctl+0x0/0x5cc) from [<800ffd44>] (sys_ioctl+0x58/0x7c)

                      |  r9:b87a8000 r8:00000000 r7:00000026 r6:00007530 r5:7e8a9fe0

                      | r4:b8d35320

                      | [<800ffcec>] (sys_ioctl+0x0/0x7c) from [<80050c00>] (ret_fast_syscall+0x0/0x30)

                      |  r8:80050d84 r7:00000036 r6:53056ee8 r5:00007530 r4:00002710

                      | Code: e594200c e5843004 e5834010 e583200c (e5823010)

                      | ---[ end trace 5847bb0f94423b98 ]---

                      | Kernel panic - not syncing: Fatal exception

                      | CPU1: stopping

                      | Backtrace:

                      | [<800543f0>] (dump_backtrace+0x0/0x10c) from [<805c7794>] (dump_stack+0x18/0x1c)

                      |  r6:00000006 r5:00000001 r4:00000000 r3:00000000

                      | [<805c777c>] (dump_stack+0x0/0x1c) from [<8004b2f8>] (do_IPI+0x104/0x1dc)

                      | [<8004b1f4>] (do_IPI+0x0/0x1dc) from [<8005092c>] (__irq_usr+0x4c/0xe0)

                      | Exception stack(0xbdaeffb0 to 0xbdaefff8)

                      | ffa0:                                     00073400 00078000 00000003 00000008

                      | ffc0: f0000000 00000000 00000000 0000f000 00000000 00000000 00073400 0000a400

                      | ffe0: 00000000 7e95b810 2acaa454 2aca79f4 20070010 ffffffff

                      |  r7:00000001 r6:00000006 r5:f2a00100 r4:ffffffff

标签 (5)
1 解答
3,288 次查看
igorpadykov
NXP Employee
NXP Employee

HI Wang

errors like "Unable to handle kernel NULL pointer dereference at virtual address"

may caused also by ddr errors, so it may be useful to run board ddr tests

i.MX6/7 DDR Stress Test Tool V2.10

Best regards

igor

在原帖中查看解决方案

4 回复数
3,289 次查看
igorpadykov
NXP Employee
NXP Employee

HI Wang

errors like "Unable to handle kernel NULL pointer dereference at virtual address"

may caused also by ddr errors, so it may be useful to run board ddr tests

i.MX6/7 DDR Stress Test Tool V2.10

Best regards

igor

3,288 次查看
denniswang_tw
Contributor II

Dear igor,

I got the same result from others, the RC should be DDR or PMIC.

I had finished the DDR stress test and the result is PASS.

Now I focus debugging on PMIC.

I will update this thread if find the RC and hope can help others.

Thanks

0 项奖励
回复
3,288 次查看
saurabh206
Senior Contributor III

Hello Wang,

Please find attached document.

It will help to debug the issue.

Also you can narrow down the issue with disabling the Wi-Fi module.

Thanks

Saurabh

3,288 次查看
denniswang_tw
Contributor II

Dear Saurabh,

Thanks for your fast reply.

I will pass information to kernel owner and hope that can help to analysis RC.

Thanks.

0 项奖励
回复