Ramdisk Kernel panic - not syncing: VFS: Unable to mount root failed i.MX6 ULL 14x14 EVK Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ramdisk Kernel panic - not syncing: VFS: Unable to mount root failed i.MX6 ULL 14x14 EVK Board

2,119 Views
Adrain
Contributor I

setenv bootargs 'console=ttymxc0,115200 initrd=0x91000040,7898116 root=/dev/ram rootwait rw init=/linuxrc';setenv ipaddr 169.254.2.194; setenv serverip 169.254.2.193;tftpboot 81000000 uImage;setenv ipaddr 169.254.2.194; setenv serverip 169.254.2.193;tftpboot 90000000 100ask_imx6ull-14x14.dtb;tftpboot 91000000 ramdisk.uImage;bootm 81000000 91000000 90000000

[ 6.388593] RAMDISK: gzip image found at block 0
[ 7.905482] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
[ 7.913798] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
[ 69.653025] Bluetooth: hci0: Failed to load rtl_bt/rtl8723b_config.bin
[ 69.659585] Bluetooth: hci0: rtl: loading rtl_bt/rtl8723b_fw.bin
[ 69.665890] bluetooth hci0: Falling back to user helper
[ 127.372847] random: crng init done
[ 131.092994] Bluetooth: hci0: Failed to load rtl_bt/rtl8723b_fw.bin

0 Kudos
Reply
2 Replies

1,963 Views
sanjayben
Contributor II

Hi,

Did you find the solution for this.

I am also facing the same

0 Kudos
Reply

1,951 Views
joanxie
NXP TechSupport
NXP TechSupport

normally this issue is related to the memory, you can check if you set this correct or not, you also can refer to the link as below:

"https://community.nxp.com/t5/i-MX-Processors/iMX6-filesystem-as-RAMdisk/m-p/295769"

0 Kudos
Reply