Radio Tuner Chip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Radio Tuner Chip

4,269 次查看
SwayamDhondge
Contributor I

I am working on android automotive 11 on imx 8 quadmax and I am exploring radio application.
As of now it seems there is no support for radio hardware on the board. 
Can anyone please provide any information regarding any Tuner chip availability which can be plugged and played.

0 项奖励
回复
4 回复数

3,285 次查看
karthik2799
Contributor I

i want to check imx8qxp board, In the board imx8qxp FM radio chipis si475x in series  FM. i need supporting drivers to play AM and FM  different frequency signals 

0 项奖励
回复

4,182 次查看
edwardtyrrell
Senior Contributor I

Hi,

A start might be to have a look in your kernel config to see if there's anything available in your specific build. In my iMX8 menuconfig I have two FM drivers, Silicon laboratories 4761/64/68 AM/FM radio and the TI WL1273 FM radio.

These are found in Device Drivers > Multifunction device drivers. Often peripherals have similar industry standard interfaces and drivers can be adapted for different families of devices. Might be worth seeing what you have already in your build, get familiar with the drivers and see what chip sets are available that may come close 'code wise'. If you have a FM chipset in mind see is there is driver source for it and try building it (with a few mods probably) and probe it in and you never know!   

Edit: Had a look at the si476x PDF and its controlled via I2C and the audio is delivered via I2S. So other chipsets are probably fairly similar. Start small, find a similar driver that has I2C and I2S, get the I2C talking, get the I2S running - job done! 

0 项奖励
回复

4,188 次查看
sooraj_ms
Contributor I

Anyone has any update on this? I am specifically looking for any FM radio module which can be plugged into the iMX8QXP MEK Board. Please help

0 项奖励
回复

4,247 次查看
swapnil
Contributor I

Hello NXP Community,

 

I am also working on a similar use case. @SwayamDhondge Did you find any such chip for the same ? 
Any help on the same will be very much appreciated.

 

Thanks in advance!

0 项奖励
回复