Radio Tuner Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radio Tuner Chip

4,315 Views
SwayamDhondge
Contributor I

I am working on android automotive 11 on imx 8 quadmax and I am exploring radio application.
As of now it seems there is no support for radio hardware on the board. 
Can anyone please provide any information regarding any Tuner chip availability which can be plugged and played.

0 Kudos
Reply
4 Replies

3,331 Views
karthik2799
Contributor I

i want to check imx8qxp board, In the board imx8qxp FM radio chipis si475x in series  FM. i need supporting drivers to play AM and FM  different frequency signals 

0 Kudos
Reply

4,228 Views
edwardtyrrell
Senior Contributor I

Hi,

A start might be to have a look in your kernel config to see if there's anything available in your specific build. In my iMX8 menuconfig I have two FM drivers, Silicon laboratories 4761/64/68 AM/FM radio and the TI WL1273 FM radio.

These are found in Device Drivers > Multifunction device drivers. Often peripherals have similar industry standard interfaces and drivers can be adapted for different families of devices. Might be worth seeing what you have already in your build, get familiar with the drivers and see what chip sets are available that may come close 'code wise'. If you have a FM chipset in mind see is there is driver source for it and try building it (with a few mods probably) and probe it in and you never know!   

Edit: Had a look at the si476x PDF and its controlled via I2C and the audio is delivered via I2S. So other chipsets are probably fairly similar. Start small, find a similar driver that has I2C and I2S, get the I2C talking, get the I2S running - job done! 

0 Kudos
Reply

4,234 Views
sooraj_ms
Contributor I

Anyone has any update on this? I am specifically looking for any FM radio module which can be plugged into the iMX8QXP MEK Board. Please help

0 Kudos
Reply

4,293 Views
swapnil
Contributor I

Hello NXP Community,

 

I am also working on a similar use case. @SwayamDhondge Did you find any such chip for the same ? 
Any help on the same will be very much appreciated.

 

Thanks in advance!

0 Kudos
Reply