Radiated emissions from Audio Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Radiated emissions from Audio Clock

1,392件の閲覧回数
ganeshskandha
Contributor I

Hi,

I have a custom board with IMX6 and SGTL5000 with Audio clock running at 11.29MHz, there are emissions from the 6th, 7th harmonics from this clock. The clock is provided by GPIO00

I have tried increasing the drive strength and controlling the slew rate with no promising effect ?

Is there any thing to be taken care in the layout/ schematics for this audio codec routing ?

Thanks,

Ganesh

ラベル(2)
0 件の賞賛
返信
1 返信

1,330件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

for decreasing emissions it is necessary to decrease drive strength and slew rate.

For layout rules one can check i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信