Radiated emissions from Audio Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radiated emissions from Audio Clock

1,394 Views
ganeshskandha
Contributor I

Hi,

I have a custom board with IMX6 and SGTL5000 with Audio clock running at 11.29MHz, there are emissions from the 6th, 7th harmonics from this clock. The clock is provided by GPIO00

I have tried increasing the drive strength and controlling the slew rate with no promising effect ?

Is there any thing to be taken care in the layout/ schematics for this audio codec routing ?

Thanks,

Ganesh

Labels (2)
0 Kudos
Reply
1 Reply

1,332 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

for decreasing emissions it is necessary to decrease drive strength and slew rate.

For layout rules one can check i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply