RTSP Streaming Internal data flow error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTSP Streaming Internal data flow error

7,361 次查看
yoheiitaya
Contributor I

Hi, community.

I tried to receive and display a RTSP Streaming from ip camera on i.MX6Q SABRE.

I tried the following GStreamer pipeline, and some cameras works fine.

# gst-launch-1.0 rtspsrc location=rtsp://192.168.100.30/profile?token=media_profile1&SessionTimeout=60 ! rtph264depay ! vpudec ! overlaysink overlay-top=384 overlay-left=512 overlay-width=512 overlay-height=384 sync=false

But on a specific camera, the following error has happened, and could not run the GStreamer.

Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Progress: (open) Opening Stream
Progress: (connect) Connecting to rtsp://192.168.100.30/profile?token=media_profile1
Progress: (open) Retrieving server options
Progress: (open) Retrieving media info
Progress: (request) SETUP stream 0
Progress: (open) Opened Stream
Setting pipeline to PLAYING ...
New clock: GstSystemClock
Progress: (request) Sending PLAY request
Progress: (request) Sending PLAY request
Progress: (request) Sent PLAY request
ERROR: from element /GstPipeline:pipeline0/GstRTSPSrc:rtspsrc0/GstUDPSrc:udpsrc1: Internal data flow error.
Additional debug info:
/home/itaya/evm/fsl-release-bsp/imx6solo/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.1-r0/gstreamer-1.4.1/libs/gst/base/gstbasesrc.c(2933): gst_base_src_loop (): /GstPipeline:pipeline0/GstRTSPSrc:rtspsrc0/GstUDPSrc:udpsrc1:
streaming task paused, reason not-linked (-1)
Execution ended after 0:00:00.077380000
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...

The error is Internal data flow error, and it seemed pipeline is not linked.

Anyone know, how to solve this problem?

Thanks.

标签 (2)
0 项奖励
回复
2 回复数

4,317 次查看
joanxie
NXP TechSupport
NXP TechSupport

I used the command as below successfully, but my rtsp from vlc, maybe you can refer to it.

gst-launch-1.0 rtspsrc location=rtsp://192.168.0.105:10000 name=source ! queue ! rtph264depay ! vpudec ! overlaysink source. ! queue ! rtpmp4gdepay ! aacparse ! beepdec ! alsasink

0 项奖励
回复

4,317 次查看
yoheiitaya
Contributor I

Thank you for reply, Guanqiong.

Sorry for reply to your comment.

I tried the command you taught me, but the result was same.

I estimate that, the real factor of this error is, the "rtspsrc" element  or anything else.

So, should I try to another pipeline element instead anything?

Payloader or videosink element are should not concerned?

Do you know any other way?

Thanks.

0 项奖励
回复