RTSP Server Setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTSP Server Setup

3,387件の閲覧回数
parveenkumaryad
Contributor III

Hi all,

I am Working on a customize project with imx6qd processor. I am using YOCTO 1.6 daisy framework. i am using linux kernel 3.10.17 .

I want to stream video+Audio from our IMX board to PC through wifi.

For that i want to set-up an RTSP-Server in our project. I am using gstreamer in the project for playing and streaming video.

I am able to stream using TCP and UDP but both of them have their own disadvantages.

Can any provide the steps to setup the server and also the gstreamer commands to stream video and audio.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,049件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you checked this discussion? It may have some useful information for you.

Regards,

Alejandro

0 件の賞賛
返信

3,049件の閲覧回数
parveenkumaryad
Contributor III

hi Alejandro

You have forget to share the link of the discussion.

Regards

Parveen

0 件の賞賛
返信

3,049件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Sorry,

RTSP gstreamer and vpudec

I hope that helps,

Alejandro

0 件の賞賛
返信