RTC driver in imx6ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC driver in imx6ull

1,681件の閲覧回数
mathew_k_t
Contributor II

Hi,

I'm using imx6ull based board. In my design, I'm using an external RTC pcf85263a.

To integrate the device, I need a driver for pcf85263a. But it is not available in the 4.1.15 Linux version.

Could you provide a Linux driver for the pcf85263a? Otherwise, suggest a suitable driver available in the above Linux version that can be used instead of pcf85263a driver.

Regards

ラベル(3)
0 件の賞賛
返信
1 返信

1,491件の閲覧回数
art
NXP Employee
NXP Employee

There is no special driver for the PCF85263A timer. You can use the regular I2C driver to access the timer.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信