Can I read/write TLP packet including 512 Bytes payload via PCIe in i.MX6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I read/write TLP packet including 512 Bytes payload via PCIe in i.MX6?

2,304 次查看
massohy
Contributor II

Dear All,

I want to read/write large TLP packet.

I read this post.

https://community.nxp.com/message/350342

It have been concluded that max payload is 128 byte.

 

I understood CX_MAX_MTU, CC_SLV_MTU and CC_MSTR_BURST_LEN are fixed.

If I change Max_Payload_Size and Max_Read_Request_Size in PCIE_RC_DConR, then can I process TLP packet including 512 byte payload with PCIe in i.MX6?

 

Best Regards,

标签 (1)
0 项奖励
回复
2 回复数

2,046 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Regarding to the PCIe RC driver contained in NXP Linux BSP, there is one outbound region used to access the CFG space of PCIe EP.The outbound TLP would be issued, when the

PCIe EP CFG IO APIs(imx_pcie_rd_conf/imx_pcie_wr_conf) are called by PCIe EP driver.

The following is the snapshot of the PCIe protocol analyzer.

one_outbound_tlp.png

One outbound TLP when the CFG space of PCIe EP is accessed.

0 项奖励
回复

2,046 次查看
massohy
Contributor II

Dear jamesbone,

 

Thank you for your reply.

I cannot decide that my understanding is correct or not, you say, driver of PCIe RC have only one region and it is for CFG space of PCIe EP, it cannot keep CFG data of PCIe RC in i.MX6. CFG space of PCIe RC in i.MX6 can be accessed only from PCIe EP, ARM CPU in i.MX6 is cannot change it.

 

That is that I cannot change Max_Payload_Size and Max_Read_Request_Size, and I cannot change max payload size of TLP packet  of PCIe in i.MX6 from 128bytes.

Do I mistake them?

Best Regards,

0 项奖励
回复