RT117x: ADIN protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT117x: ADIN protection

ソリューションへジャンプ
1,680件の閲覧回数
ak2
Contributor I

Hi,

Does the analog input pin with
   VREFH = 1.8V,
   CSACAL = 1 and
   3V3 GPIO_NVCC mode
need a protection against voltage levels above 1.8V or is a protection for values above 3.96V sufficient?

Thanks for the help!

0 件の賞賛
返信
1 解決策
1,674件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ak2 ,

   From the RT1170RM, we can know some information:

kerryzhou_0-1655780263059.png

But, if you define CSACAL = 1, then it is Full scale (Factor of 1), 

kerryzhou_1-1655780300878.png

So, the input voltage should follow this table:

kerryzhou_2-1655780440844.png

can't above 1.8V, thanks.

If the CSACAL = 0, you can input 3.3V.

Wish it helps you!

Best Regards,

Kerry

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,675件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ak2 ,

   From the RT1170RM, we can know some information:

kerryzhou_0-1655780263059.png

But, if you define CSACAL = 1, then it is Full scale (Factor of 1), 

kerryzhou_1-1655780300878.png

So, the input voltage should follow this table:

kerryzhou_2-1655780440844.png

can't above 1.8V, thanks.

If the CSACAL = 0, you can input 3.3V.

Wish it helps you!

Best Regards,

Kerry

 

 

 

0 件の賞賛
返信
1,664件の閲覧回数
ak2
Contributor I

Thank you!

As you mention, I will set CSCALE to 0.

0 件の賞賛
返信