RT1176 crash on SEMC init with high M7 core frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 crash on SEMC init with high M7 core frequency

1,445 Views
raddeh
Contributor III

Trying to initialise the SEMC when the M7 core runs with a high clock frequency does lead to a crash of the CPU that I can't recover from (even JTAG doesn't work anymore). A power-cycle is required.

I have set up access to an external SRAM and an exteran SDRAM. Both access work when having the M7 core clock configured to 336 MHz and the SEMC clock to 198 MHz (no SEMC configuration patch). Changing the configured M7 core frequency of the project to 672 MHz does lead to the aforementioned crash.

All clocks are configured once on startup:

SEMC clock config from the MCUXpresso Config Tools:

raddeh_0-1665667302800.png

Working M7 core clock config:

raddeh_1-1665667349250.png

 

Core M7 clock config that leads to the crash:

raddeh_2-1665667377522.png

 

 

The SEMC is configured for SRAM as follows:

void ext_sram_semc_init(void)
{
    uint64_t root_clock_hz = CLOCK_GetRootClockFreq(kCLOCK_Root_Semc);
    double clock_cycles_per_ns;
    semc_config_t sdk_base_config;
    semc_sram_cs_t sram_cs_pin;
    semc_sram_config_t sdk_sram_config;

    memset(&sdk_base_config, 0, sizeof(semc_config_t));
    SEMC_GetDefaultConfig(&sdk_base_config);
    SEMC_Init(SEMC, &sdk_base_config);

    memset(&sdk_sram_config, 0, sizeof(semc_sram_config_t));
    sram_cs_pin = kSEMC_SRAM_CS0;
    sdk_sram_config.address = 0x98000000;
    sdk_sram_config.cePinMux = kSEMC_MUXCSX0;
    sdk_sram_config.memsize_kbytes = (512 * 16) / 8; // 8MBit = 512*16*1KBits = 1MB
    sdk_sram_config.addrPortWidth  = 19; //Address pins A0..A18
    sdk_sram_config.advActivePolarity = kSEMC_AdvActiveLow;
    sdk_sram_config.addrMode = kSEMC_AddrDataNonMux;
    sdk_sram_config.burstLen = kSEMC_Nor_BurstLen1;
    sdk_sram_config.portSize = kSEMC_PortSize16Bit;
    sdk_sram_config.syncMode = kSEMC_AsyncMode;
    sdk_sram_config.waitEnable = false;
    sdk_sram_config.waitSample = false;
    sdk_sram_config.advLevelCtrl = kSEMC_AdvLow;
    sdk_sram_config.tCeSetup_Ns        = 0;
    sdk_sram_config.tCeHold_Ns         = 3;
    sdk_sram_config.tCeInterval_Ns     = 10;
    sdk_sram_config.readHoldTime_Ns    = 0xFF;
    sdk_sram_config.tAddrSetup_Ns      = 0;
    sdk_sram_config.tAddrHold_Ns       = 10;
    sdk_sram_config.tWeLow_Ns          = 8;
    sdk_sram_config.tWeHigh_Ns         = 0;
    sdk_sram_config.tReLow_Ns          = 6;
    sdk_sram_config.tReHigh_Ns         = 5;
    sdk_sram_config.tTurnAround_Ns     = 3;
    sdk_sram_config.tAddr2WriteHold_Ns = 0;
    sdk_sram_config.tWriteSetup_Ns     = 0;
    sdk_sram_config.tWriteHold_Ns      = 0;
    sdk_sram_config.latencyCount       = 0;
    sdk_sram_config.readCycle          = 0;
    sdk_sram_config.delayChain         = 10;

    SEMC_ConfigureSRAMWithChipSelection(SEMC, sram_cs_pin, &sdk_sram_config, root_clock_hz);
}

 

Why does the CPU crash hard when I use the higher M7 core frequency and try to init the SEMC? The SEMC SDK function calls does finish but the crash happens immediately afterwards. How can I prevent the crash?

Tags (2)
0 Kudos
Reply
2 Replies

1,435 Views
jay_heng
NXP Employee
NXP Employee

Can you please share your project linker file? are you debugging project in XIP Flash? or maybe Internal RAM?

0 Kudos
Reply

1,424 Views
raddeh
Contributor III

The program is running only in internal flash. XIP isn't used. This here is the linker file:

 

/* Entry Point */
ENTRY(Reset_Handler)

/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size  = 0;      /* required amount of heap              */
_Min_Stack_Size = 0x200;  /* required amount of stack 0x200 = 512 */

/* Memory areas */
MEMORY
{
    m_flexspi_itcm  (RX) : ORIGIN = 0x00000000, LENGTH = 0x00040000
    m_flexspi_dtcm  (RW) : ORIGIN = 0x20000000, LENGTH = 0x00040000
    m_ocram         (RW) : ORIGIN = 0x202C0000, LENGTH = 0x00080000
}

/* Define output sections */
SECTIONS
{
    /* Interrupt vectors, startup code -> start of ITCM */
    .interrupts :
    {
        __VECTOR_TABLE = .;
        __Vectors = .;
        . = ALIGN(4);
        KEEP(*(.isr_vector))     /* Startup code */
        . = ALIGN(4);
    } > m_flexspi_itcm

    /* Program code behind ISR & startup */
    .text :
    {
        . = ALIGN(4);
        *(.text)                 /* .text sections (code) */
        *(.text*)                /* .text* sections (code) */
        *(.glue_7)               /* glue arm to thumb code */
        *(.glue_7t)              /* glue thumb to arm code */

        KEEP (*(.init))
        KEEP (*(.fini))

        . = ALIGN(4);
        _etext = .;        /* define a global symbols at end of code */
    } > m_flexspi_itcm

    .ARM.extab :
    {
        *(.ARM.extab* .gnu.linkonce.armextab.*)
    } > m_flexspi_itcm

    .ARM :
    {
        __exidx_start = .;
        *(.ARM.exidx*)
        __exidx_end = .;
    } > m_flexspi_itcm

    __etext = .;    /* define a global symbol at end of code */
    __DATA_ROM = .; /* Symbol is used by startup for data initialization */
    __VECTOR_RAM = ORIGIN(m_flexspi_itcm);
    __RAM_VECTOR_TABLE_SIZE_BYTES = 0x0;

    __TEXT_END = .; /* End of text section */
    text_end = ORIGIN(m_flexspi_itcm) + LENGTH(m_flexspi_itcm);
    ASSERT(__TEXT_END <= text_end, "region m_flexspi_itcm overflowed with text")

    /* Strings and constants into OCRAM */
    .text2 :
    {
        . = ALIGN(4);
        *(.rodata)               /* .rodata sections (constants, strings, etc.) */
        *(.rodata*)              /* .rodata* sections (constants, strings, etc.) */

        . = ALIGN(4);
        _etextrodata = .;        /* define a global symbols at end of code */
    } > m_ocram

    __TEXT_END2 = .; /* End of text section */
    ocram_end = ORIGIN(m_ocram) + LENGTH(m_ocram);
    ASSERT(__TEXT_END2 <= ocram_end, "region m_ocram overflowed with text")

    /* Initialised data */
    .data : AT(__DATA_ROM)
    {
        . = ALIGN(4);
        __DATA_RAM = .;
        __data_start__ = .;      /* create a global symbol at data start */
        *(m_usb_dma_init_data)
        *(.data)                 /* .data sections */
        *(.data*)                /* .data* sections */
        KEEP(*(.jcr*))
        . = ALIGN(4);
        __data_end__ = .;        /* define a global symbol at data end */
    } > m_flexspi_dtcm
    __NDATA_ROM = __DATA_ROM + (__data_end__ - __data_start__);

    /* Uninitialised data */
    .bss :
    {
        /* This is used by the startup in order to initialize the .bss section */
        . = ALIGN(4);
        __START_BSS = .;
        __bss_start__ = .;
        *(m_usb_dma_noninit_data)
        *(.bss)
        *(.bss*)
        *(COMMON)
        . = ALIGN(4);
        __bss_end__ = .;
        __END_BSS = .;
    } > m_flexspi_dtcm

    PROVIDE ( end = __bss_end__ );
    PROVIDE ( _end = __bss_end__ );

    __NCACHE_REGION_START = ORIGIN(m_ocram);
    __NCACHE_REGION_SIZE  = 0;

    /* Heap + Stack section, used to check that there is enough RAM left */
    .heap_stack :
    {
      . = ALIGN(4);
      . = . + _Min_Heap_Size;
      . = . + _Min_Stack_Size;
      . = ALIGN(4);
      __heap_stack_ = .;
    } > m_flexspi_dtcm

    /* Initializes stack on the end of block */
    __StackTop   = ORIGIN(m_flexspi_dtcm) + LENGTH(m_flexspi_dtcm);
    PROVIDE(__stack = __StackTop);

    .ARM.attributes 0 : { *(.ARM.attributes) }

    ASSERT(__heap_stack_ <= __StackTop, "region m_flexspi_dtcm overflowed with data, stack and heap")

    /* Remove information from the standard libraries */
    /DISCARD/ :
    {
      libm.a ( * )
      libc.a ( * )
      libgcc.a ( * )
    }

}

 

 

0 Kudos
Reply