RT1170 development board SDK added using C++ static library issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170 development board SDK added using C++ static library issues

1,001件の閲覧回数
jianwuQuan
Contributor I

Due to project development requirements, additional C++ static libraries were added to the RT1170 SDK for use. The current one is MCUXpresso IDE V11.5.1_726.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

987件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Note that you need to set Library search path and name in MCUX project option after adding file into project folder

MCUX_Make_Lib_Use_Static_Library.PNG

0 件の賞賛
返信

994件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @jianwuQuan ,

Yes, can add c++ library to a c++ project in MCUXpresso IDE. And it's no problem on RT1170 EVK.

Please refer to chapter 16 in MCUXpresso_UDE_User_Guide.pdf which can be found in IDE's folder.

Regards,

Jing

0 件の賞賛
返信