RT1170 binary load using C-SPY utility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 binary load using C-SPY utility

1,429 Views
AhmedHabib
NXP Employee
NXP Employee

Hi,

I am using MIMXRT1170-EVK Board, uart example for cm7.

I am trying to load the binary on the target using the cspy tool (through lpuart_polling_cm7.debug.cspy.bat). It loads and running as expected but keeps the command line open and it never terminates until ended by user.

I tried to add argument --download_only for the .out file, it loads the image but not execute it until I attach using IAR and press Go.

My questions:

1. How to use the cspy tool to load the binary image and execute it without any manual intervention? 

2. How to add script to let the target execute it I used --download_only option? Here I am using CMSIS-DAP connection?

 

The uart project which is part of RT1170 SDK is attached.

Snipped from the scripts:

"C:\iar\ewarm-9.60.2\common\bin\cspybat" -f "lpuart_polling_cm7.debug.general.xcl" --backend -f "lpuart_polling_cm7.debug.driver.xcl"
C:\iar\ewarm-9.60.2\arm\bin\armPROC.dll

 C:\iar\ewarm-9.60.2\arm\bin\armJET.dll

 --download_only ..\Debug\lpuart_polling_cm7.out

 --plugin=C:\iar\ewarm-9.60.2\arm\bin\armLibSupportUniversal.dll

 --device_macro=C:\iar\ewarm-9.60.2\arm/config/debugger/NXP/iMXRT_1170.dmac

 --device_macro=C:\iar\ewarm-9.60.2\arm/config/debugger/NXP/iMXRT_1170_cm7.dmac

 --device_macro=C:\iar\ewarm-9.60.2\arm/config/debugger/NXP/iMXRT_1170_FlexSPI.dmac

 --macro=C:\Users\nxg00411\Downloads\MIMXRT1170-EVK-lpuart_polling_cm7\lpuart_polling_cm7/evkmimxrt1170/evkmimxrt1170_connect_cm7.mac

 --flash_loader=C:\iar\ewarm-9.60.2\arm/config/flashloader/NXP/FlashIMXRT1170_FlexSPI.board
--endian=little

--cpu=Cortex-M7

--fpu=VFPv5_D16

-p

C:\iar\ewarm-9.60.2\arm\config\debugger\NXP\MIMXRT1176xxxA_M7.ddf

--semihosting

--device=MIMXRT1176xxxA_M7

--multicore_nr_of_cores=1

--jet_probe=cmsisdap

--jet_standard_reset=1,0,0

"--reset_style=\"0,-,0,Disabled__no_reset_\""

"--reset_style=\"1,SoftwareReset,1,Software\""

"--reset_style=\"2,-,0,Hardware\""

"--reset_style=\"3,CoreReset,0,Core\""

"--reset_style=\"4,-,0,System\""

--drv_interface=SWD

--drv_catch_exceptions=0x800

--jet_board_cfg=C:\iar\ewarm-9.60.2\arm/config/debugger/NXP/IMXRT1170.ProbeConfig




Regards,

Ahmed Habib

Labels (1)
0 Kudos
Reply
1 Reply

1,408 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @AhmedHabib ,

 

The C-SPY macros might help you on this purpose, for example, 

Kan_Li_0-1728533397302.pngKan_Li_0-1728533397302.png

Please kindly refer to https://wwwfiles.iar.com/RX/webic/doc/EWRX_DebuggingGuide.ENU.pdf for more details.

 

Please kindly contact IAR for further support. https://www.iar.com/about/contact 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply