RT1062 doesn't make it to "Main" loop during debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1062 doesn't make it to "Main" loop during debug

2,322件の閲覧回数
tpetrovic
Contributor I

I am using the RT1062 on a custom PCB. It is using external flash chip IS25LP128F-JKLE and external SDRAM MT48LC16M16A2P. I am using a J-Link Base to program the device.

I am trying to run the "hello world" demo using MCUXpresso IDE and the SDK "SDK_2.x_EVK-MIMXRT1060". Since external flash is larger than what is used on the eval board (MIMXRT1060-EVK), I changed the size and frequency values in "evkmimxrt1060_flexspi_nor_config.c" as shown in the attached image.

When I start the debug, the code never reaches the "main" loop, and doesn't allow me to step through code. When I pause the program, it seems to always be stuck at 0x20ed48.

I'm hoping to get some help as to why the program would be getting stuck before the "main" loop. Are there additional parameters I need to change for the larger Flash size? I attached some screenshots for clarity, but let me know if you need further information. 

0 件の賞賛
返信
2 返答(返信)

2,192件の閲覧回数
vaibhavkambli
Contributor I

@tpetrovic, Did you find any solution.

I am also facing similar issue. Please help if possible.

タグ(1)
0 件の賞賛
返信

2,186件の閲覧回数
tpetrovic
Contributor I

Hi @vaibhavkambli ,

My software team was able to find a solution. I believe they used a different IDE or programmer to completely erase the chip. After that, I had no problem executing and debugging the code. Best of luck! I'll let you know if I dig up any more details. 

タグ(1)
0 件の賞賛
返信