RT1050 x CMOS Image Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 x CMOS Image Sensor

ソリューションへジャンプ
3,953件の閲覧回数
rubensjunior
Contributor IV

Dear collegues,

I would like an example of communication, for example I2C, of the RT1050 family processor with a CMOS image sensor, for example the BF3901CS (BYD Manufacturer) sensor.
Can someone help me?

Have a great day!

Rubens Júnior

ラベル(1)
1 解決策
3,787件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thanks for your reply.
Regarding the camera interface, please refer to page 15 in the attachment.

pastedImage_1.jpg

Fig 1 Camera interface

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,787件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There're some CSI demos in the SDK library, it presents how to receive the camera data using CSI driver.
These code demos are suited for the OV7725 and MT9M114, please refer to them for details.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,787件の閲覧回数
rubensjunior
Contributor IV

Hello jeremyzhou‌,

Thank you so much for your return. Please send us a connection diagram of the IMXRT1050-EVKB board with the camera?

Thanks a lot!

Best Regards.

Rubens Júnior.

0 件の賞賛
返信
3,788件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thanks for your reply.
Regarding the camera interface, please refer to page 15 in the attachment.

pastedImage_1.jpg

Fig 1 Camera interface

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------