RT patch for linux 3.0.35 on IM.X6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT patch for linux 3.0.35 on IM.X6

1,433 Views
hongjunsong
Contributor I

Hi,

We are using IM.X6 with linux 3.0.35 from freescale for our real time application.  We found out the linux3.0.35 kernel cannot meet our real time requirements.  We are trying to apply the RT patch from https://rt.wiki.kernel.org/index.php/Main_Page​.  Once we applied the RT 3.0.35 patch for the freescale 3.0.35 linux, and found out that there are some files which cannot be patched.  We manually updated these files, and could build the kernel image.  However, the built kernel cannot run.

Later on, we found out the Freescale 3.0.35 is slight different from the official linux 3.0.35.  We would like to know anybody here could share any thought on this.

Regards,

Hongjun

Labels (7)
0 Kudos
Reply
1 Reply

1,219 Views
igorpadykov
NXP Employee
NXP Employee

Hi hongjun

for differencies one can look at

What the FSL Community BSP is not

FSL Community BSP Release Notes 1.8 documentation

also recommended to post this to meta-fsl-arm mailing list, so that more

people could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply