RS232 connection not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS232 connection not working

1,322 Views
MarkoPanger
Contributor III

Hi all,

I've just received the i.MX53 QSB board. I've inserted the supplied SD card, and RS232 cable and power up the board. I can see uboot booting and counting down 3s before booting up the kernel.

Unfortunately I can't prevent uboot from booting the kernel as uboot doesn't accept any input from my keyboard. I'm using minicom. I'm sure my connection to PC is working fine as if I just swap the 53QSB board for a i.mx51 EVK it works as it should.

The same happens if I let the kernel boot up. When it comes to entering the username and password I just can't enter anything through the RS232 connection.

Is this a know issue with i.mx53QSB ?

Thanks, Marko

Labels (1)
0 Kudos
Reply
2 Replies

1,246 Views
AlanLevy
Contributor I

The RS232 interface on the QSB should work in both directions. You should check that you've got the right RS232 cable and that minicom is configured correctly - in particular there's no hardware handshaking.

0 Kudos
Reply

1,246 Views
MarkoPanger
Contributor III

Got it working. It was a soldering problem on the connector. Thank, Marko.

0 Kudos
Reply