I have a custom board with a 8Mplus Toradex SOM.
I was looking at the file:
arch/arm64/boot/dts/freescale/imx8mp-evk-rpmsg.dts
To try and copy the relevant parts to enable the RPMSG drivers on the SOM
When I copy this section over to my custom device tree:
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
m4_reserved: m4@0x80000000 {
no-map;
reg = <0 0x80000000 0 0x1000000>;
};
vdev0vring0: vdev0vring0@55000000 {
compatible = "shared-dma-pool";
reg = <0 0x55000000 0 0x8000>;
no-map;
};
vdev0vring1: vdev0vring1@55008000 {
compatible = "shared-dma-pool";
reg = <0 0x55008000 0 0x8000>;
no-map;
};
vdevbuffer: vdevbuffer@55400000 {
compatible = "shared-dma-pool";
reg = <0 0x55400000 0 0x100000>;
no-map;
};
rsc-table {
reg = <0 0x550ff000 0 0x1000>;
no-map;
};
audio_reserved: audio@0x81000000 {
compatible = "shared-dma-pool";
no-map;
reg = <0 0x81000000 0 0x10000000>;
};
};
The board fails to boot and I see this message in the Uboot log:
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
ERROR: reserving fdt memory region failed (addr=550ff000 size=1000)
ERROR: Failed to allocate 0x38000 bytes below 0x100000000.
device tree - allocation error
FDT creation failed! hanging...### ERROR ### Please RESET the board ###
I know this is a Toradex module (and I'm posting this on their forum as well) but this looks like it is more a problem with the NXP device tree.
I'm curious why the nodes related to the RPMSG on the imx8mplus-evk-rpmsg.dts still have the names as "m4" instead of a m7, since the co-processor on a imx8mplus is a M7 not a M4.
Any help will greatly appreciated, thanks!