RPMSG, Increasing number of buffer (RPMSG_NUM_BUFS)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RPMSG, Increasing number of buffer (RPMSG_NUM_BUFS)

22,267 次查看
niranjanbc
Contributor IV

below are the changes i have made in imx_rpmsg.c file

#define RPMSG_NUM_BUFS (1024)
+#define RPMSG_BUF_SIZE (512)
+#define RPMSG_BUFS_SPACE (RPMSG_NUM_BUFS * RPMSG_BUF_SIZE)
+
+/*
+ * The alignment between the consumer and producer parts of the vring.
+ * Note: this is part of the "wire" protocol. If you change this, you need
+ * to update your BIOS image as well
+ */
+#define RPMSG_VRING_ALIGN (4096)
+.

.

.

.

.

struct imx_rpmsg_vproc *rpdev = &imx_rpmsg_vprocs[i];
+
+ if (!strcmp(rpdev->rproc_name, "m4")) {
+ ret = of_device_is_compatible(np, "fsl,imx7d-rpmsg");
+ ret |= of_device_is_compatible(np, "fsl,imx6sx-rpmsg");
+ if (ret) {
+ /* hardcodes here now. */
+ rpdev->vring[0] = 0xBF800000;//0xBFFF0000;
+ rpdev->vring[1] = 0xBF880000;//0xBFFF8000;
+ }
+ } else {
+ break;
+ }

i want to increase the number of buffers, what other changes i have to make that work.

if change the buffer number back to 512, i see rpmsg driver works fine.with above memory allocation.

i have allocated now last 8MB of shared DDR  memory for RPMSG.

do i need to change "RPMSG_VRING_ALIGN", what is the value and how to calculate it.

if i change RPMSG_VRING_ALIGN, what other files are affected, what other changes i have to make.

标签 (2)
标记 (1)
0 项奖励
回复
29 回复数

4,029 次查看
b50844
NXP Employee
NXP Employee

Hi Niranjanbc,

Yes, you are.
In RPMsg Lite, the init function does not block and you need to check whether the link is up by an explicit call.
Also, you need to announce a new "channel" creation to the other side so that the kernel modules on the linux dies get probed.

Something in this way:

    my_rpmsg = rpmsg_lite_remote_init((void *)startupData, RPMSG_LITE_LINK_ID, RL_NO_FLAGS);

 
    while (!rpmsg_lite_is_link_up(my_rpmsg))  ;
 
    my_queue = rpmsg_queue_create(my_rpmsg);
    my_ept = rpmsg_lite_create_ept(my_rpmsg, LOCAL_EPT_ADDR, rpmsg_queue_rx_cb, my_queue);
    rpmsg_ns_bind(my_rpmsg, app_nameservice_isr_cb);
    rpmsg_ns_announce(my_rpmsg, my_ept, RPMSG_LITE_NS_ANNOUNCE_STRING, RL_NS_CREATE);
 
    PRINTF("\r\nNameservice sent, ready for incoming messages...\r\n");
 
    for (;;)
    {
        /* Get RPMsg rx buffer with message */
        result = rpmsg_queue_recv_nocopy(my_rpmsg, my_queue, (unsigned long *)&remote_addr, (char **)&rx_buf, &len,
                                         RL_BLOCK);
.
.
.

Hope it helped,
Regards,
Marek

0 项奖励
回复

4,029 次查看
niranjanbc
Contributor IV

Hi Marek

I tried has below, still no luck

struct rpmsg_lite_instance *rpmsgM4Instance;
rpmsg_queue_handle rpmsgQ;
void* rpmsg_lite_base = BOARD_SHARED_MEMORY_BASE;
struct rpmsg_lite_endpoint *ctrl_ept;

....

.

.

.

env_init();


rpmsgM4Instance  =  rpmsg_lite_remote_init(rpmsg_lite_base, RL_PLATFORM_IMX6SX_M4_LINK_ID,                                                              RL_NO_FLAGS);


while(!rpmsg_lite_is_link_up(rpmsgM4Instance));

PRINTF("RPMSG Lite Initialized\n\r");

rpmsgQ = rpmsg_queue_create(rpmsgM4Instance);


ctrl_ept = rpmsg_lite_create_ept(rpmsgM4Instance, RL_ADDR_ANY, rpmsg_queue_rx_cb, rpmsgQ);

rpmsg_ns_bind(rpmsgM4Instance, app_namservice_callback);

rpmsg_ns_announce(rpmsgM4Instance, ctrl_ept, "rpmsg-openamp-demo-channel", RL_NS_CREATE);

for (;;)
{
rpmsg_queue_recv_nocopy(rpmsgM4Instance, rpmsgQ, &src, &rx_buf, &len, 0xFFFFFFFF);
.

.

.

.

.
rpmsg_queue_nocopy_free(rpmsgM4Instance, rx_buf);
}

0 项奖励
回复

4,029 次查看
b50844
NXP Employee
NXP Employee

Hi Niranjanbc,

Is your BOARD_SHARED_MEMORY_BASE setup correctly?

Can you please generate a patch with your changes in Linux kernel and your application for the M4 side and share it here? I think I could look into it more and help you.

Also, you can try to add more pr_error() in Linux and more PRINTF in the M4 app and you can copy here the dmesg printout from kernel and output of M4 console...

Regards,
Marek

0 项奖励
回复

4,029 次查看
niranjanbc
Contributor IV

Hi Marek,

below please find the dmesg log and attached patch kernel

dmesg
Booting Linux on physical CPU 0x0
Linux version 3.14.28-1.0.0_ga+g91cf351 (niranjan@niranjan) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Wed Jun 21 14:18:59 EDT 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 SoloX Honeywell PIM Board
cma: CMA: reserved 320 MiB at aa000000
Memory policy: Data cache writealloc
On node 0 totalpages: 258048
free_area_init_node: node 0, pgdat 80b31940, node_mem_map be757000
  DMA zone: 2016 pages used for memmap
  DMA zone: 0 pages reserved
  DMA zone: 258048 pages, LIFO batch:31
PERCPU: Embedded 8 pages/cpu @be739000 s8832 r8192 d15744 u32768
pcpu-alloc: s8832 r8192 d15744 u32768 alloc=8*4096
pcpu-alloc: [0] 0  
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 256032
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw uart_from_osc
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 682860K/1032192K available (5344K kernel code, 259K rwdata, 5568K rodata, 252K init, 387K bss, 349332K reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xbf800000 - 0xff000000   (1016 MB)
    lowmem  : 0x80000000 - 0xbf000000   (1008 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x80ab052c   (10914 kB)
      .init : 0x80ab1000 - 0x80af0280   ( 253 kB)
      .data : 0x80af2000 - 0x80b32c40   ( 260 kB)
       .bss : 0x80b32c4c - 0x80b93960   ( 388 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 256 kB
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
clocksource_of_init: no matching clocksources found
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x805165c0 - 0x80516618
Brought up 1 CPUs
SMP: Total of 1 processors activated.
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1100 mV  
vdd3p0: 2800 <--> 3150 mV at 3000 mV  
vdd2p5: 2100 <--> 2875 mV at 2500 mV  
cpu: 725 <--> 1450 mV at 1150 mV  
vddpcie-phy: 725 <--> 1450 mV  
vddsoc: 725 <--> 1450 mV at 1175 mV  
syscon 20e4000.iomuxc-gpr: regmap [mem 0x020e4000-0x020e7fff] registered
imx_mmdc_probe: failed to enable automatic power saving
imx-mmdc: probe of 21b0000.mmdc failed with error -16
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
syscon 21ac000.romcp: regmap [mem 0x021ac000-0x021affff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6sx-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
20dc000.gpc supply pu not found, using dummy regulator
MU is ready for cross core communication!
bio: create slab <bio-0> at 0
mxs-dma 1804000.dma-apbh: initialized
VCC_SD3: 3000 mV  
PSU-5V0: 5000 mV  
vref-3v3: 3300 mV  
usb_otg1_vbus: 5000 mV  
usb_otg2_vbus: 5000 mV  
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usbphy_nop1.12 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-3: IMX I2C adapter registered
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
RPMSG_RING_SIZE Niranjan: 12288
PAGE_SIZE Niranjan: 4096
imx_rpmsg_probe rpdev0: vring0 0xbf7f0000, vring1 0xbf7f8000
virtio_rpmsg_bus virtio0: rpmsg host is online
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
Compressor "zlib", prio 60
Compressor "zlib", prio 60
Compressor "rtime", prio 50
fuse init (API version 7.22)
JFS: nTxBlock = 7894, nTxLock = 63158
msgmni has been set to 1973
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight.17 supply power not found, using dummy regulator
MIPI DSI driver module loaded
2224000.lcdif supply lcd not found, using dummy regulator
mxsfb 2224000.lcdif: registered mxc display driver ldb
DISPLAY: Power-on latency exceeded, new value 481333 ns
DISPLAY: Power-off latency exceeded, new value 27000 ns
Console: switching to colour frame buffer device 128x37
DISPLAY: Power-off latency exceeded, new value 28667 ns
mxsfb 2224000.lcdif: initialized
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze3000 found.
SW1A: 700 <--> 1475 mV at 1375 mV  
SW1B: 700 <--> 1475 mV at 1375 mV  
SW2: 2500 <--> 3300 mV at 3300 mV  
SW3: 900 <--> 1650 mV at 1350 mV  
SWBST: 5000 <--> 5150 mV at 5000 mV  
VSNVS: 1000 <--> 3000 mV at 3000 mV  
VREFDDR: 750 mV  
VLDO1: 1800 <--> 3300 mV at 3300 mV  
VLDO2: 800 <--> 1550 mV at 1500 mV  
VCCSD: 2850 <--> 3300 mV at 3300 mV  
V33: 2850 <--> 3300 mV at 3000 mV  
VLDO3: 1800 <--> 3300 mV at 3300 mV  
VLDO4: 1800 <--> 3300 mV at 1800 mV  
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 1500000) is a IMX
console [ttymxc0] enabled
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 1500000) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs-pwrkey as /devices/soc0/soc.0/2000000.aips-bus/20cc000.snvs-pwrkey/input/input0
snvs_pwrkey 20cc000.snvs-pwrkey: i.MX snvs powerkey probed
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc2: no vqmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
galcore: clk_get 2d core clock failed, disable 2d/vg!
Galcore version 5.0.11.25762
usb 1-1: new high-speed USB device number 2 using ci_hdrc
mmc2: host does not support reading read-only switch. assuming write-enable.
mmc2: new high speed SDHC card at address 59b4
mmcblk2: mmc2:59b4 USD   7.47 GiB  
 mmcblk2: p1 p2
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
mmc3: BKOPS_EN bit is not set
mmc3: switch to highspeed failed
mmc3: new MMC card at address 0001
mmcblk3: mmc3:0001 P1XXXX 3.60 GiB  
mmcblk3boot0: mmc3:0001 P1XXXX partition 1 2.00 MiB
mmcblk3boot1: mmc3:0001 P1XXXX partition 2 2.00 MiB
mmcblk3rpmb: mmc3:0001 P1XXXX partition 3 128 KiB
 mmcblk3: unknown partition table
 mmcblk3boot1: unknown partition table
 mmcblk3boot0: unknown partition table
ax88179_178a 1-1:1.0 eth0: register 'ax88179_178a' at usb-ci_hdrc.1-1, ASIX AX88179 USB 3.0 Gigabit Ethernet, d8:eb:97:b7:37:08
wm8962 3-001a: Failed to read ID register
wm8962: probe of 3-001a failed with error -110
fsl-asrc 2034000.asrc: driver registered
imx6sx-pinctrl 20e0000.iomuxc: pin MX6SX_PAD_SD4_DATA4 already requested by 219c000.usdhc; cannot claim for 2004000.spdif
imx6sx-pinctrl 20e0000.iomuxc: pin-164 (2004000.spdif) status -22
imx6sx-pinctrl 20e0000.iomuxc: could not request pin 164 (MX6SX_PAD_SD4_DATA4) from group spdifgrp  on device 20e0000.iomuxc
fsl-spdif-dai 2004000.spdif: Error applying setting, reverse things back
imx-wm8962 sound.24: audmux internal port setup failed
imx-wm8962: probe of sound.24 failed with error -22
imx-spdif sound-spdif.25: snd-soc-dummy-dai <-> 2004000.spdif mapping ok
TCP: cubic registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
A9-M4 sema4 num 6, A9-M4 magic number 0x12345678 - 0x4f4d4213.
SWBST: disabling
usb_otg1_vbus: disabling
vref-3v3: disabling
PSU-5V0: disabling
regulator-dummy: disabling
gpio-keys gpio-keys.19: Button without keycode: 0x6a
gpio-keys: probe of gpio-keys.19 failed with error -22
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
ALSA device list:
  #0: imx-spdif
EXT3-fs (mmcblk2p2): warning: mounting fs with errors, running e2fsck is recommended
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk2p2): using internal journal
EXT3-fs (mmcblk2p2): recovery complete
EXT3-fs (mmcblk2p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 252K (80ab1000 - 80af0000)
udevd[82]: starting version 182
evbug: Connected device: input0 (20cc000.snvs-pwrkey at snvs-pwrkey/input0)
random: nonblocking pool is initialized
Blank Screen: Setting LCD backlight to 0
CPUFreq Utilities: Setting interactive CPUFreq governor
CPU0
CPUFreq Utilities: Setting 792000 CPUFreq Max Scaling Freq
CPUFreq Utilities: Setting 198000 CPUFreq Min Scaling Freq
DISPLAY: Power-off latency exceeded, new value 69333 ns
DISPLAY: Power-off latency exceeded, new value 1081666 ns
file system registered

0 项奖励
回复

4,029 次查看
b50844
NXP Employee
NXP Employee

Hi Niranjan,

I cannot see the print-outs with "niranjan" string anywhere in the patch, are you sure you include everything?
Also, could you add more PRINTs in the M4 application and post here the printouts from M4? 

I would also suggest, if possible, to first test RPMsg Lite with default VRING addresses and then to change the addresses in Linux and on M4 side, so that we make one change per step... 

Thanks,
Marek

0 项奖励
回复

4,029 次查看
niranjanbc
Contributor IV

i didnt add any print errors yet, i just attached patch and dmesg thinking that code might already have print error messages.

i am attaching m4 side FreeRtos code as well

the value for BOARD_SHARED_MEMORY_BASE 

#define BOARD_SHARED_MEMORY_BASE  ((void*)0xBF7F0000)

i am attaching IAR linker file as well. 

Printf message from M4

rpmsg_lite_remote_init: sucess
rpmsg_queue_create: success
rpmsg_lite_create_ept: success
rpmsg_ns_bind: success
rpmsg_ns_announce: success

0 项奖励
回复

4,029 次查看
niranjanbc
Contributor IV

thanks for the clarification Marek, i will work on porting to RPMsg-lite. 

0 项奖励
回复

4,029 次查看
b36401
NXP Employee
NXP Employee

You can refer these RPMsg examples:
https://community.nxp.com/docs/DOC-333803

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,029 次查看
niranjanbc
Contributor IV

Hi Victor,

thanks for sharing the link, but i dont find any information/example related to increasing buffer and dependencies.

can you point me to right document, if i am missing anything.

my main problem is, if increase buffer number. RPMSG is not working.

thanks

Niranjan 

0 项奖励
回复