RPA tool - how to generate "relaxed" LPDDR4 timing?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RPA tool - how to generate "relaxed" LPDDR4 timing?

跳至解决方案
872 次查看
frank_vanhooft
Contributor III

What's the best way to use the RPA spreadsheet tool to create "relaxed" LPDDR4 timing? By that I mean timings with more than the usual margin, to allow for more (component / temp / etc) variabilities?

I can think of two possible ways, but I don't know if one is better than the other, or even valid.

1. Specify a lower "clock cycle frequency" eg 1400 MHz instead of the default 1500 MHz. Then put a corresponding value in the "DDR Stress Test File" tab DRAM_PLL_FDIV_CTL0 register cell for that frequency. So the bus runs at 1400 MHz using 1400 MHz timing values.

2. Leave the clock cycle frequency at 1500 MHz, and generate the register values for that. But edit the "DDR Stress Test File" tab DRAM_PLL_FDIV_CTL0 register cell for a lower freq, eg 1400 MHz. So the iMX8 runs the bus at 1400 MHz but uses 1500 MHz timing values.

Any comments or suggestions?

Thanks.

0 项奖励
回复
1 解答
701 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

@frank_vanhooft Here you need use the method 1 to generate timing.

If you want to change DDR clock, you should use new frequency DDR configuration and clock setting both at same time.

Hope this can do help for you

在原帖中查看解决方案

0 项奖励
回复
5 回复数
845 次查看
frank_vanhooft
Contributor III

In my question above, is either option, 1 or 2, better than the other? Or is there another, better, third option?

Thanks.

0 项奖励
回复
832 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will help confirm, which product are you using, i.MX8MP or others?

0 项奖励
回复
782 次查看
frank_vanhooft
Contributor III

iMX8 Mini,  the MIMX8MM6DVTLZAA  

Thanks.

0 项奖励
回复
702 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

@frank_vanhooft Here you need use the method 1 to generate timing.

If you want to change DDR clock, you should use new frequency DDR configuration and clock setting both at same time.

Hope this can do help for you

0 项奖励
回复
851 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复