RPA tool - how to generate "relaxed" LPDDR4 timing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RPA tool - how to generate "relaxed" LPDDR4 timing?

Jump to solution
870 Views
frank_vanhooft
Contributor III

What's the best way to use the RPA spreadsheet tool to create "relaxed" LPDDR4 timing? By that I mean timings with more than the usual margin, to allow for more (component / temp / etc) variabilities?

I can think of two possible ways, but I don't know if one is better than the other, or even valid.

1. Specify a lower "clock cycle frequency" eg 1400 MHz instead of the default 1500 MHz. Then put a corresponding value in the "DDR Stress Test File" tab DRAM_PLL_FDIV_CTL0 register cell for that frequency. So the bus runs at 1400 MHz using 1400 MHz timing values.

2. Leave the clock cycle frequency at 1500 MHz, and generate the register values for that. But edit the "DDR Stress Test File" tab DRAM_PLL_FDIV_CTL0 register cell for a lower freq, eg 1400 MHz. So the iMX8 runs the bus at 1400 MHz but uses 1500 MHz timing values.

Any comments or suggestions?

Thanks.

0 Kudos
Reply
1 Solution
699 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@frank_vanhooft Here you need use the method 1 to generate timing.

If you want to change DDR clock, you should use new frequency DDR configuration and clock setting both at same time.

Hope this can do help for you

View solution in original post

0 Kudos
Reply
5 Replies
843 Views
frank_vanhooft
Contributor III

In my question above, is either option, 1 or 2, better than the other? Or is there another, better, third option?

Thanks.

0 Kudos
Reply
830 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will help confirm, which product are you using, i.MX8MP or others?

0 Kudos
Reply
780 Views
frank_vanhooft
Contributor III

iMX8 Mini,  the MIMX8MM6DVTLZAA  

Thanks.

0 Kudos
Reply
700 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@frank_vanhooft Here you need use the method 1 to generate timing.

If you want to change DDR clock, you should use new frequency DDR configuration and clock setting both at same time.

Hope this can do help for you

0 Kudos
Reply
849 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply