RMII based level Translator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RMII based level Translator

1,924件の閲覧回数
niteshsahay
Contributor III

Hi

Can i use NTB0104  for the level translation of RMII signals.

But this translator supports upto 100Mbps.If not so please suggest Automotive grade Level translator for RMII.

Regards

Nitesh

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,747件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nitesh Kumar,

The NTB0104-Q100 does have the Q100 (Grade 1) certification. However, it won’t support the full speed of the RMII interface, as you can see on the product datasheet below.

http://www.nxp.com/documents/data_sheet/NTB0104_Q100.pdf

There are several voltage translators available but I would recommend looking for a RMII focused solution due to the speed of RMII.

https://www.nxp.com/documents/brochure/75017511.pdf

I hope this helps!

Regards,

1,747件の閲覧回数
niteshsahay
Contributor III

Hi

Thanks for the reply.

Can you suggest me the Voltage level Translator for RMII application.

Regrdas

Nitesh

0 件の賞賛
返信