RMII based level Translator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII based level Translator

2,008 Views
niteshsahay
Contributor III

Hi

Can i use NTB0104  for the level translation of RMII signals.

But this translator supports upto 100Mbps.If not so please suggest Automotive grade Level translator for RMII.

Regards

Nitesh

Labels (2)
0 Kudos
Reply
2 Replies

1,831 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nitesh Kumar,

The NTB0104-Q100 does have the Q100 (Grade 1) certification. However, it won’t support the full speed of the RMII interface, as you can see on the product datasheet below.

http://www.nxp.com/documents/data_sheet/NTB0104_Q100.pdf

There are several voltage translators available but I would recommend looking for a RMII focused solution due to the speed of RMII.

https://www.nxp.com/documents/brochure/75017511.pdf

I hope this helps!

Regards,

1,831 Views
niteshsahay
Contributor III

Hi

Thanks for the reply.

Can you suggest me the Voltage level Translator for RMII application.

Regrdas

Nitesh

0 Kudos
Reply