RMII PHY on i.MX8MP with external reference clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII PHY on i.MX8MP with external reference clock

2,707 Views
benpicco
Contributor II

Hello,

we are connecting a KSZ8091RNA PHY to the i.MX8MP processor found on the phyCORE-i.MX8MP module using the RMII interface.

The PHY is generating the reference clock, but when I configure the i.MX8MP to not generate the reference clock by adding snps,rmii_refclk_ext to the eqos device tree node, the MAC does not receive the input clock:

 

 

 

[    5.052963] imx-dwmac 30bf0000.ethernet eth1: PHY [stmmac-1:00] driver [Micrel KSZ8081 or KSZ8091] (irq=POLL)
[    6.069309] imx-dwmac 30bf0000.ethernet: Failed to reset the dma
[    6.075355] imx-dwmac 30bf0000.ethernet eth1: stmmac_hw_setup: DMA engine initialization failed
[    6.084129] imx-dwmac 30bf0000.ethernet eth1: stmmac_open: Hw setup failed

 

 

 

 When I remove the snps,rmii_refclk_ext option the interface comes up, but it looks like the PHY and the MAC both generate the reference clock on separate pins and can't exchange Ethernet data:

 

 

 

[    2.247814] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51
[    2.254640] imx-dwmac 30bf0000.ethernet:     DWMAC4/5
[    2.259453] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported
[    2.266597] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported
[    2.273740] imx-dwmac 30bf0000.ethernet: TX Checksum insertion supported
[    2.280449] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported
[    2.286603] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[    2.294270] imx-dwmac 30bf0000.ethernet: Enabled Flow TC (entries=8)
[    2.300638] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[    2.308214] imx-dwmac 30bf0000.ethernet: Using 34 bits DMA width
[    5.242914] imx-dwmac 30bf0000.ethernet eth1: PHY [stmmac-1:00] driver [Micrel KSZ8081 or KSZ8091] (irq=POLL)
[    5.259271] imx-dwmac 30bf0000.ethernet eth1: No Safety Features support found
[    5.266580] imx-dwmac 30bf0000.ethernet eth1: IEEE 1588-2008 Advanced Timestamp supported
[    5.277944] imx-dwmac 30bf0000.ethernet eth1: registered PTP clock
[    5.292434] imx-dwmac 30bf0000.ethernet eth1: configuring for phy/rmii link mode
[    8.382960] imx-dwmac 30bf0000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx

 

 

 

But no data is received and when I send something, I don't see any packets in Wireshark on a 2nd machine connected via Ethernet

 

 

 

eth1      Link encap:Ethernet  HWaddr 50:2D:F4:24:67:4A  
          inet6 addr: fe80::522d:f4ff:fe24:674a/64 Scope:Link
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:738 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:118312 (115.5 KiB)
          Interrupt:44 

 

 

 

 

My 'working' device tree is 

 

 

 

 

&eqos {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_eqos>;
        phy-mode = "rmii";
        phy-handle = <&ethphy1>;
        status = "okay";

//      snps,rmii_refclk_ext;

        mdio {
                compatible = "snps,dwmac-mdio";
                #address-cells = <1>;
                #size-cells = <0>;

                ethphy1: ethernet-phy@0 {
                        compatible = "ethernet-phy-ieee802.3-c22";
                        reg = <0x0>;
                };
        };
};

&iomuxc {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_hog>;

        pinctrl_eqos: eqosgrp {
                fsl,pins = <
                        MX8MP_IOMUXC_ENET_MDC__ENET_QOS_MDC             0x2
                        MX8MP_IOMUXC_ENET_MDIO__ENET_QOS_MDIO           0x2
                        MX8MP_IOMUXC_ENET_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x16
                        MX8MP_IOMUXC_ENET_TD0__ENET_QOS_RGMII_TD0       0x16
                        MX8MP_IOMUXC_ENET_TD1__ENET_QOS_RGMII_TD1       0x16
                        MX8MP_IOMUXC_ENET_RXC__ENET_QOS_RX_ER           0x90
                        MX8MP_IOMUXC_ENET_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x90
                        MX8MP_IOMUXC_ENET_RD0__ENET_QOS_RGMII_RD0       0x90
                        MX8MP_IOMUXC_ENET_RD1__ENET_QOS_RGMII_RD1       0x90
                        MX8MP_IOMUXC_ENET_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK      0x4000001f
                >;
        };
};

 

 

 

tbh I have no idea how those pinctrl values are determined - I just copied them from other boards and they don't match the IOMUXC registers from the data sheet - so what are they?

 I understand that MX8MP_IOMUXC_ENET_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK must be the crucial value here, but how do I configure it as input?

 

Thank you for your help!

Tags (3)
0 Kudos
Reply
3 Replies

2,646 Views
benpicco
Contributor II

Thank you for confirming that the configuration should behave as expected - it turned out to be a hardware issue: CRS_DV / RXCTL and REF_CLK were not connected correctly. (We had it on TXCK instead of TD2)

With the PHY wired up properly things are working fine now.

0 Kudos
Reply

2,634 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @benpicco,

I hope you are doing well
 
Glad to know that query has been resolved. If there is no further query should I mark this thread as closed?
 
Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply

2,659 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @benpicco,

Q) but it looks like the PHY and the MAC both generate the reference clock on separate pins and can't exchange Ethernet data:
=> Here, The device tree seems correct. Please share your schematics for further debugging the issue.
 
Q) I have no idea how those pinctrl values are determined
=>The pinctrl values should be configured as per the pad control registers from the reference manual.
i,e. For ENET_MDIO, the properties like slew rate, pull up, open drain, etc.. can be configured according to section 8.2.4.170 SW_PAD_CTL_PAD_ENET_MDIO SW PAD Control Register from the reference manual IMX8MPRM.
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply