RF antenna PCB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RF antenna PCB

1,752件の閲覧回数
idom
Contributor II

Hi 

in the i.MX 8M Mini LPDDR4 EVK, There is RF antenna PCB glued.

Can I have the design or at least the UG  of it.

Does it support 5GHz?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,623件の閲覧回数
romitchatterjee
Contributor V

Hello Ido, the on-board Wi-Fi module from Murata supports 5 GHz - I have tested it. As for the antenna, perhaps you can find some information in the schematics here: i.MX 8M Mini Evaluation Kit | NXP  ?

0 件の賞賛
返信

1,623件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ido

for rf and antenna design one can ask additional documentation on wifi vendor portal

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信