RC can not write data to i.MX6SX(EP) again

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RC can not write data to i.MX6SX(EP) again

877 Views
袁增兴
Contributor I

Frankly speaking, when we put i.MX6SX into EP mode, we find that RC can only write the data to i.MX just one time. The procedure is, firstly i.MX is configured the bar size(bar 0/1 64bit 8M), then RC will pcie scan all the devices including i.MX, finally i.MX will do the BAR0/1 inbound mapping using BAR matching, and i.MX doesn't work well in inbound address matching mode.

We find RC can succeed to write the data to i.MX, but fail to access to i.MX the other time, can anyone provide some help?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

791 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please check EP mode examples on

https://community.freescale.com/docs/DOC-95014 

for narrowing down problem may be recommended try to reproduce issue

on i.MX6SX Sabre boards.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply