RC can not write data to i.MX6SX(EP) again

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RC can not write data to i.MX6SX(EP) again

882 次查看
袁增兴
Contributor I

Frankly speaking, when we put i.MX6SX into EP mode, we find that RC can only write the data to i.MX just one time. The procedure is, firstly i.MX is configured the bar size(bar 0/1 64bit 8M), then RC will pcie scan all the devices including i.MX, finally i.MX will do the BAR0/1 inbound mapping using BAR matching, and i.MX doesn't work well in inbound address matching mode.

We find RC can succeed to write the data to i.MX, but fail to access to i.MX the other time, can anyone provide some help?

Thanks

标签 (1)
0 项奖励
回复
1 回复

796 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please check EP mode examples on

https://community.freescale.com/docs/DOC-95014 

for narrowing down problem may be recommended try to reproduce issue

on i.MX6SX Sabre boards.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复