RAM Test using UUU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM Test using UUU

3,082件の閲覧回数
ankitpanchal167
Contributor III

Hi,

I want to perform a RAM test on imx8mp using UUU utility. Can you please provide any references to meet our expectations? 

I have already tested the imx6ull processer and we found some options to test 'rdmem' and 'wrmem' commands in UUU to test RAM memory but for the imx8mp it is not available.

UUU version : 1.4.193
Uboot-imx version : 2021.0

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,023件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ankitpanchal167,

I hope you are doing well.

Yes, As per the uuu script I tried to run the command to read and write in the memory but it skipped the command and jumped to the SDPU command sequence.

The SDP commands will only be run when the machine is i.MX6/7/8MM/8MQ.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

3,017件の閲覧回数
ankitpanchal167
Contributor III
Yes, right SDP commands are not working with imx8mp. I want to test RAM memory using UUU.
Is there any way to test RAM memory using UUU?
Like, push some binary on board. And test RAM and give the results.
0 件の賞賛
返信

2,989件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ankitpanchal167,


I hope you are doing well.

It appears there is no way as the support is not given itself in i.MX8MP.
I suggest using DDR tool for i.MX8mp with that one can do RAM testing along with calibration, and stress test.

Please find it in the below link.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

It will be helpful.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信