RAM Memory usage measurement tool for iMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM Memory usage measurement tool for iMX6Q

1,364件の閲覧回数
nthiru28
Contributor I

Hello NXP,

I'm using iMX6Q processor with the BSP provided and developed many application in c/c++. Now i want measure the usage of RAM by each application with modules wise not just USS or PSS and also need to detect memory leaks at run time.

Please suggest me some tool with document.

Regards,

Thiru N

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,286件の閲覧回数
art
NXP Employee
NXP Employee

First, you can use some generic debug tools, such as GDB/KGDB. Please refer to the following Application Note:

http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Then, please just search the internet, there are many open source monitoring/debugging tools for Linux. For example, look here:

http://www.tecmint.com/command-line-tools-to-monitor-linux-performance/


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信