R8169 driver issue when connecting via SSH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

R8169 driver issue when connecting via SSH

730 Views
bamontales
Contributor I

We are currently testing the kernel version, lf-6.1.55-2.2.1 from the linux-imx repository. But we are encountering an issue with the ethernet driver, Realtek R8169, when connecting via SSH. This driver is working on older version which is rel_imx_5.4.70_2.3.7.

The chip we are using is i.MX6 Quad.

Here is the kernel message encountered.

[   61.995657] ------------[ cut here ]------------
[   61.995691] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:526 dev_watchdog+0x1c8/0x1cc
[   61.995740] NETDEV WATCHDOG: eth1 (r8169): transmit queue 0 timed out
[   61.995757] Modules linked in: binfmt_misc r8169 imx_sdma nfnetlink [last unloaded: configfs]
[   61.995851] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.55 #5
[   61.995868] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[   61.995885]  unwind_backtrace from show_stack+0x10/0x14
[   61.995924]  show_stack from dump_stack_lvl+0x40/0x4c
[   61.995947]  dump_stack_lvl from __warn+0xb0/0xd4
[   61.995966]  __warn from warn_slowpath_fmt+0xa4/0x1d0
[   61.995983]  warn_slowpath_fmt from dev_watchdog+0x1c8/0x1cc
[   61.996007]  dev_watchdog from call_timer_fn.constprop.5+0x18/0x80
[   61.996050]  call_timer_fn.constprop.5 from run_timer_softirq+0x43c/0x460
[   61.996082]  run_timer_softirq from __do_softirq+0x148/0x2b0
[   61.996110]  __do_softirq from irq_exit+0xc4/0x100
[   61.996135]  irq_exit from call_with_stack+0x18/0x20
[   61.996158]  call_with_stack from __irq_svc+0x90/0xc8
[   61.996174] Exception stack(0x80f01ea8 to 0x80f01ef0)
[   61.996190] 1ea0:                   00000000 00000002 00000001 80f09ec0 00000001 00000001
[   61.996203] 1ec0: 80f0c338 00000001 6ba7edff 6f3a265d daf098f8 0000000e 00000000 80f01ef8
[   61.996214] 1ee0: 809590d4 806ecf60 20070013 ffffffff
[   61.996223]  __irq_svc from cpuidle_enter_state+0x170/0x37c
[   61.996252]  cpuidle_enter_state from cpuidle_enter+0x28/0x38
[   61.996276]  cpuidle_enter from do_idle+0x1e0/0x258
[   61.996300]  do_idle from cpu_startup_entry+0x18/0x1c
[   61.996316]  cpu_startup_entry from rest_init+0xd8/0xdc
[   61.996335]  rest_init from arch_post_acpi_subsys_init+0x0/0x8
[   61.996382] ---[ end trace 0000000000000000 ]---

 

Labels (1)
0 Kudos
Reply
1 Reply

689 Views
pengyong_zhang
NXP Employee
NXP Employee

hI, @bamontales 

Did you change anything about the BSP code?

0 Kudos
Reply