R10.4 c_patch problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

R10.4 c_patch problem

ソリューションへジャンプ
2,429件の閲覧回数
charleschang
Contributor III

I follow user guild, when I run c_patch, it want me to confirm that it need to remove 3 folder in first, includes kernel_imx,

I say yes, then It compain about there are not files in kernel_imx.

So I modify the "baseversion" , about the kernel_imx entry, chage the "NEW" to "CHANGE".

It works!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,070件の閲覧回数
charleschang
Contributor III

something wrong in the file: baseversion.

when you run c_patch , it failed on some project, 

for example, the kernel_imx project, 

you need to modify the "baseverion" file, change the entry of kernel_imx from "NEW" to "CHANGE"

muthe srinivas said:

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,071件の閲覧回数
charleschang
Contributor III

something wrong in the file: baseversion.

when you run c_patch , it failed on some project, 

for example, the kernel_imx project, 

you need to modify the "baseverion" file, change the entry of kernel_imx from "NEW" to "CHANGE"

muthe srinivas said:

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

0 件の賞賛
返信
2,070件の閲覧回数
muthesrinivas
Contributor I

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

0 件の賞賛
返信