R10.4 c_patch problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

R10.4 c_patch problem

Jump to solution
2,443 Views
charleschang
Contributor III

I follow user guild, when I run c_patch, it want me to confirm that it need to remove 3 folder in first, includes kernel_imx,

I say yes, then It compain about there are not files in kernel_imx.

So I modify the "baseversion" , about the kernel_imx entry, chage the "NEW" to "CHANGE".

It works!

Labels (1)
0 Kudos
Reply
1 Solution
2,084 Views
charleschang
Contributor III

something wrong in the file: baseversion.

when you run c_patch , it failed on some project, 

for example, the kernel_imx project, 

you need to modify the "baseverion" file, change the entry of kernel_imx from "NEW" to "CHANGE"

muthe srinivas said:

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

View solution in original post

0 Kudos
Reply
2 Replies
2,085 Views
charleschang
Contributor III

something wrong in the file: baseversion.

when you run c_patch , it failed on some project, 

for example, the kernel_imx project, 

you need to modify the "baseverion" file, change the entry of kernel_imx from "NEW" to "CHANGE"

muthe srinivas said:

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

0 Kudos
Reply
2,084 Views
muthesrinivas
Contributor I

can you explain it in detail.please?

I am getting problem with c_patch  for the same R10.4 can u explain it again in detail,,,plz!

0 Kudos
Reply