Questions about using DMIC on RT1170-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about using DMIC on RT1170-EVK

ソリューションへジャンプ
2,348件の閲覧回数
Shawn_
Contributor I

Hello everyone,

I want to learn to use the four DMICs on RT1170-EVK, but I can't find any examples of DMICs and driver files like fsl_dmic.c and fsl_dmic.h in SDK2.11.0. Does NXP have some introduction and Demos for DMIC on RT1170?

Thanks and Regards

ラベル(2)
0 件の賞賛
返信
1 解決策
2,341件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Shawn_ ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   To the RT1170, it doesn't use the DMIC IP, it is using the PDM ad the DMIC IP.

   Please refer to this code:

\SDK_2_11_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\pdm\pdm_sai_multi_channel_edma

  It will use the EVK on board U40,U41 DMIC.

kerryzhou_0-1646278228386.png

So, your used driver is fsl_pdm, fsl_pdm_edma.

 

Wish it helps you!

Best Regards,

Kerry

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,342件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Shawn_ ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   To the RT1170, it doesn't use the DMIC IP, it is using the PDM ad the DMIC IP.

   Please refer to this code:

\SDK_2_11_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\pdm\pdm_sai_multi_channel_edma

  It will use the EVK on board U40,U41 DMIC.

kerryzhou_0-1646278228386.png

So, your used driver is fsl_pdm, fsl_pdm_edma.

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 件の賞賛
返信