Questions about the i.MX6UL Reference Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the i.MX6UL Reference Design

1,198 Views
agodeau
Contributor III

We are looking to add some components to the reference design of the i.MX6UL/NXP Modular Gateway for a  project and have some clarification questions:

Have there been any revisions or update to the NXP reference design since Schematic Revision 2.05?

Which ports are open/available for use?

 Is everything going to being connected through the SO-DIMM Connector Interface(Base Board Schematic pg.7)?

What is the maximum current draw in amps for the 5V input power supply interface (Base Board Schematic pg.3)?

What is the maximum current draw in amps for the 3.3V SW regulator Interface (Base Board Schematic pg.3)?

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,125 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Aquiel Godeau ,

   i.MX6UL/NXP Modular Gateway is designed by 3rd party, See here, please!

https://www.nxp.com/webapp/connect/displayPartnerProfile.sp?partnerId=8660

So please contact them!

Have a nice day!

BR,

weidong

0 Kudos
Reply