Questions about i.MX6 SD & SDIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about i.MX6 SD & SDIO

1,235件の閲覧回数
宗標廖
Contributor V

Hello Community

I have some quetions about i.MX6 SD & SDIO

1)Is it L3.0.35_4.1.0 support SD3.0 UHS-I mode?

In i.MX_6Dual6Quad_SABRE-AI_Linux_Release_Notes for L3.0.35_4.1.0, there is description as bellow:

ushdc-ltib.PNG

But I did a test with an UHS-I SD card on i.mx6qsabreauto board with BSP 3.0.35_4.1.0,the card did not enter

USH-I mode(I am sure the related configs are right).On the otherhand,the Yocto BSP is OK.

2)According to the snapshot above, L3.0.35_4.1.0 does not support SDIO3.0 specification, is it right?

Best Regards

ZongbiaoLiao

ラベル(2)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

I think you are right, this release does not support SD3.0.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信