Question regarding i.MX6 IPU display interface scan order

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question regarding i.MX6 IPU display interface scan order

1,789 Views
liuhao
Contributor I

I am new to i.MX6 and currently I am reading i.MX6 datasheet (iMX6DQPRM.pdf) and I have a question regarding IPU display interface (DI). In chapter 37.1.2.1.2.2 Display Interface, it mentioned:

The interface includes the following additional features:
• Screen size: up to 4096 x 2048 pixels, programmable by software.
• Scan Order: progressive or interlaced
• Synchronization
• Programmable horizontal and vertical synchronization output signals (for
synchronous access)
• Data enabling output signal
• Software contrast control using 8-bit programmable pulse-width modulation (PWM)
Two dedicated PWM outputs are provided

The video data in memory is progressive 30 fps 24 bits RGB data in memory. However I would like to output interlaced video signal via a TV encoder. Therefore I would like to output interlaced RGB data to display interface. Can I use scan order of interlaced to do this?

Also, each IPU has two display interface. Can I use scan order interlaced to one display interface and progressive to another display interface?

Many thanks in advance.

0 Kudos
Reply
2 Replies

1,521 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, it can be supported, the interlaced display patch: Patch for iMX6 BSP to support interlaced display on HDMI and LCD interface

0 Kudos
Reply

1,522 Views
liuhao
Contributor I

Thank you very much for the info. Very helpful.

0 Kudos
Reply