Question, patch code for i.MX6Q AndroidBSP4.0 known issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, patch code for i.MX6Q AndroidBSP4.0 known issue

1,529件の閲覧回数
Aemj
Contributor IV

Hi all,

My customer is using your AndroidBSP4.0(ICS) for their own board.

And they saw the reboot could fail during their repeated reboot test.

Because the following is written as ‘ known issue’ in the release note of Android4.0, they believe the issue is related to that.

“The loopback reboot tests may cause failure”

There is no similar description in the release note of AndroidBSP4.3.

Can I understand the known issue, the loopback reboot tests may cause failure, was solved in AndroidBSP4.3?

If so, can you provide the patch code for the AndroidBSP4.0 to solve the issue?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,495件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi AVNET,

All the patch you can see are under the  Updates and Patches (12) of  i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale​ .

Here I recommend you to use the newest version BSP.

Hope this can help you.
Have a great day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,495件の閲覧回数
Aemj
Contributor IV

Hi Dan,

Thanks for your comment.

Could you show me what patch can solve the reboot issue in R13.4-GA for Android 4.0.4?

And could you show me whether the reboot issue has been solved in the latest AndroidBSP?

Thanks,

Miyamoto

0 件の賞賛
返信