Question on i.MX6's PCIe RX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on i.MX6's PCIe RX

2,662 Views
t_kuha
Contributor I

Hi,

I have a problem in receiving data over PCIe from EP device. (TX is Okay.)

How can I know the RX status?

Is there any register (or something like that) for debugging?

Regards,

Tags (2)
0 Kudos
Reply
3 Replies

2,443 Views
igorpadykov
NXP Employee
NXP Employee

Hi t_kuha

in general may be recommended to perform pcie compliance tests:

QA: About i.Mx6 PCIe compliance 

How to setup i.MX6Dual/Quad and i.MX6Solo/DualLite Linux software for PCIe compliance Test? 

I am afraid there is no way to know the RX status from i.MX6 side, except measuring its level with special equipment.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,443 Views
t_kuha
Contributor I

igor,

Thank you for the reply.

Is there any examples of i.MX6 (RC) receiving Memory Write TLP from EP device?

Regards,

0 Kudos
Reply

2,443 Views
igorpadykov
NXP Employee
NXP Employee

Hi t_kuha

one can look at examples on

https://community.nxp.com/docs/DOC-95014 

Best regards
igor

0 Kudos
Reply