Question on hog in device tree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on hog in device tree

3,555 Views
christophe
Contributor V

Hi all,

I have a trouble with pin "hogging" in a particular case, and no explanation about it.

I have a camera chip connected to an imx6q through spi. The chip needs 4 gpios to work (GPIO2_28, GPIO3_19, GPIO3_20 and GPIO5_0). All these gpio are named in ecspi2 structure, and pin are declared in pinctrl_gschip.

For me, it would be enough to make the chip work... But it's not the case, since the GPIO2_28, set up in the chip driver, has no level change at all.

To make it work, i have to also declare the pin in iomuxc structure. In this case, the GPIO2_28 is fully operationnal.

Do you see some explanation about this issue ?

&ecspi2 {
    fsl,spi-num-chipselects = <1>;
    cs-gpios = <&gpio2 26 0>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi2>;
    status = "okay";

  gschip: gschip@0 {
    compatible = "gn,gschip";
    reg = <0>;
    pinctrl-0 = <&pinctrl_gschip>;
    mclk = <74500000>;
    mclk_src = <0>;
    ipu= <0>;
    csi = <0>;
    spi-max-frequency = <20000000>;
    reset-gpio = <&gpio2 28 0>;
    sdi_lock-gpio = <&gpio3 19 0>;
    rate_det-gpio = <&gpio3 20 0>;
    data_err-gpio = <&gpio5 0 0>;
    };
};

    pinctrl_gschip: gschipgrp {
      fsl,pins = <
        MX6QDL_PAD_EIM_EB0__GPIO2_IO28            0x1b0b1
        MX6QDL_PAD_EIM_D19__GPIO3_IO19            0x1b0b1
        MX6QDL_PAD_EIM_D20__GPIO3_IO20            0x1b0b1
        MX6QDL_PAD_EIM_WAIT__GPIO5_IO00           0x1b0b1
      >;
    };

&iomuxc {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_hog>;

    imx6qdl-starlitehd {
        pinctrl_hog: hoggrp {
            fsl,pins = <
        MX6QDL_PAD_EIM_EB0__GPIO2_IO28            0x1b0b1   /* Reset Gennum */
            >;
        };

Best regards,

Christophe

Labels (1)
4 Replies

2,972 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Christophe,

The hog pins should be used for those pins that are not controlled by any particular driver.

In your usecase the 'gn,gschip' driver should request and control the GPIOs accordingly.

Regards,

Fabio Estevam

2,972 Views
christophe
Contributor V

Hi Fabio,

I agree with you. This pin is used by 'gn,gschip' driver. But it is actually not drived if not declared in hog.

I assume it's a bug in device tree.

Rgds,

Christophe

0 Kudos
Reply

2,972 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Christophe Cholet,

I was doing some research as this behavior seemed odd. However, it is possible that the gschip@0 node is lacking the pintrl-names definition. Would you please try adding it before the pinctrl-0 definition? Let us know if it helps

Would look like:

pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gschip>;

I hope this helps!

 

Regards,

0 Kudos
Reply

2,972 Views
christophe
Contributor V

Hi gusarambula,

Adding pinctrl-0 has no effect. Pin still must be in hog.

Rgds,

Christophe

0 Kudos
Reply