Question of about ASRC use method

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question of about ASRC use method

ソリューションへジャンプ
1,639件の閲覧回数
felixhsu
Contributor III


Hi all

I have some question about Asynchronous Sample Rate Converter (ASRC),

Q1:

If use ASRC convert I2S clock, LRCLK will follow BCLK frequency convert or not ?

Q2:

In the document  i.MX_6_Linux_Reference_Manual Chapter 31 (ASRC) explanation ASRC have two use case,

case 1: Memory > ASRC > Memory

case 2: Memory > ASRC > peripheral

the use case can be convert to peripheral > ASRC > peripheral or not ? if yes how to change setting.

Q3:

If connection the phone with Bluetooth, can be transmission the voice data at the same time ?

PS: Bluetooth use 8K Hz sample rate and audio codec use 48K Hz sample rate, so the ASRC must convert 8K Hz to 48K Hz at the input voice data and convert 48K Hz to 8K Hz at the output voice data.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

1. yes

2. no. One can try implement this in own codes using mentioned examples

3. yes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,269件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

1. yes

2. no. One can try implement this in own codes using mentioned examples

3. yes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信