Question of DDR3 Script Aid(i.MX6DQ)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question of DDR3 Script Aid(i.MX6DQ)

2,072 Views
hyunhoshin
Contributor III

There are 2 version of DDR3 Script Aid(excel file, for i.MX6DQ)

"I.MX6DQSDL DDR3 Script Aid V0.10.xlsx" and "I.MX6DQSDL DDR3 Script Aid V0.11.xlsx"

What's the difference between the two?

Labels (1)
0 Kudos
Reply
3 Replies

1,867 Views
joanxie
NXP TechSupport
NXP TechSupport

0.11 version add note for duty cycle consideration.

0 Kudos
Reply

1,867 Views
hyunhoshin
Contributor III

I set the same DDR parameters in each document(I.MX6DQSDL DDR3 Script Aid V0.10.xlsx,I.MX6DQSDL DDR3 Script Aid V0.11.xlsx)

However, there are differenct value of the output as shown below.


*I.MX6DQSDL DDR3 Script Aid V0.10.xlsx
setmem /32 0x021b0008 = 0x09444040 // MMDC0_MDOTC

*I.MX6DQSDL DDR3 Script Aid V0.11.xlsx
setmem /32 0x021b0008 = 0x24444040 // MMDC0_MDOTC

I set the same DDR parameter, but I don't know why this value is different.

What is the correct value of MMDC0_MDOTC register?

0 Kudos
Reply

1,867 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as below, what's the difference about tAOFPD  and tAONPD, you can check your DDR's data sheet

https://community.nxp.com/thread/435651 

0 Kudos
Reply